×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109747584, Entry date: 12/08/2017
(0)
Rate

.NET application for the SIMATIC RF350M with WiFi connection (inclusive SDK)

  • Entry
  • Associated product(s)
The hand-held terminal SIMATIC RF350M is designed for the flexible use of radio frequency identification (RFID). The device is based on Windows CE and therefore offers the opportunity to create and use individual, user-specific applications for RFID cheaply and in a standardized way.

An SDK is offered to create own applications for the RF350M, which maps all available RFID functions. It also contains an API for the native implementation via C++ and another API for the Microsoft .NET Compact Framework.

This application example shows a customized application of RFID based on the .NET API created with C#, that demonstrates the basic functions of RFID. This includes reading, writing, stocktaking and initialization of transponders as well as the opportunity to switch the read head regarding the available air interfaces RF300 and ISO15693.

In addition, the example shows how to use the integrated WiFi interface of the RF350M to send read out transponder data to a PC or a S7‑PLC.



Documentation and example project
  Documentation (9.2 KB)

 Registrierung notwendig Sample application for the SIMATIC RF350M (Visual Studio 2005) (96,0 KB)
SHA-256 Checksum: 0E74C984674DDF3692EE02A268141AE9F3D39A50CB898CAB39F393238C4CB19A

 Registrierung notwendig Sample application for Windows to receive transponder data (Visual Studio 2005) (51,1 KB)
SHA-256 Checksum: 007946EAC3801734D1F0DA7EF193FA0C8A49B88C5E0B6B1E8BC2CF28504F31A0

 Registrierung notwendig Sample application for an S7 PLC to receive transponder data (TIA Portal V14 SP1)  (1,6 MB)

 Registrierung notwendig RF350M .NET SDK (7,2 MB)
SHA-256 Checksum: 2B33AF799E07ED311E632D719B9275287DFC8B7BD48765394A70E2670E71F03C

You can find Informations to SHA-256 at the entry
How do you determine the SHA-256 checksum of a file?


Additional Keywords
 
SDK, API, DotNet

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.