×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109747647, Entry date: 10/23/2017
(1)
Rate

Emergency stop shutdown to SIL 2 or PL c with a contactor with F-PLC-IN and fail-safe controller

  • Entry
  • Associated product(s)
Single-channel emergency stop shutdown of a motor by a fail-safe controller and 3RT1 power contactor with fail-safe control.

Emergency stop shutdown to SIL 2 or PL c with a contactor with F-PLC-IN and fail-safe controller

Operating principle

The fail-safe controller monitors the emergency stop device.

When the emergency stop device is actuated, the fail-safe controller switches the power contactor off by means of its fail-safe input (F-PLC-IN) in a safety-related way.

If the emergency stop device is unlatched and the feedback circuit is closed, the Start button can be used to switch on again.

Note

Please note that the hardware fault tolerance (HFT) must also be observed in addition to the PFHd values for the SIL when using the contactor with an F-PLC-IN acc. to IEC 62061. In this example, SIL 2 is achieved, but due to the HFT of 0, welding of the contactor contacts can lead to a loss of the safety function.

The mirror contact of the contactor is used for fault diagnostics and must be monitored in the higher-level application (evaluation unit) in order to be able to initiate appropriate response in the event of a fault. 

For example, a circuit-breaker can be used here as the second shutdown path. More information is available in the following FAQ: Which Safety Integrity Level can be achieved using a contactor and a circuit breaker?  40349715

When transferring this example as a subsystem to a complete application acc. to ISO 13849, the architecture of the subsystem and common cause failures (CCF) must also be taken into account in order to obtain the corresponding PL. This means that it is not possible to directly transfer a SIL to a PL.

 Registrierung notwendig  SET_Emergency_stop_SIL2_3RT1_F-PLC-IN_F-CPU_en.zip (7,1 KB)

 Registrierung notwendig  TIA_Portal_Emergency_stop_SIL2_3RT1_F-PLC-IN_F-CPU.zip (2,2 MB)

 Registrierung notwendig  Wiring_Emergency_stop_SIL2_3RT1_F-PLC-IN_F-CPU.zip (60,5 KB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.