×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109747990, Entry date: 10/23/2018
(5)
Rate

When do you need a "Hardware Support Package" (HSP) to integrate the SITOP PSU8600 / SITOP UPS1600 into the TIA Portal?

  • Entry
  • Associated product(s)
Due to the new hardware and firmware versions the SITOP PSU8600 power supply system and the SITOP UPS1600 uninterruptible power supply with PROFINET interface are no longer included in the hardware catalog of various versions of TIA Portal and therefore have to be retro-installed via a hardware support package (HSP).

The Hardware Support Packages (HSPs) will permit you to configure modules that are not contained in the hardware catalog of your TIA Portal installation. Install the HSP for SITOP PSU8600 and SITOP UPS1600 according to the version of the TIA Portal.

  • SITOP PSU8600: HSP 0103
  • SITOP UPS1600: HSP 0063

The HSPs for integration in the TIA Portal are in Entry ID 72341852.

Check whether the version of the HSP installed is the latest version. If not, install the latest HSP. This is described in Entry ID:54163658.

For TIA Portal V14 and higher, the SITOP PSU8600 power supply system with basic devices, expansion modules and buffer modules as well as the SITOPUPS1600 uninterruptible power supply with basic devices and battery modules (SITOP UPS1100) are permanent items in the hardware catalog.


Fig. 01

The following table shows which devices with which firmware can be parameterized in which version of TIA Portal. The requirement here is that the corresponding HSP is installed insofar as the devices are not or are not yet available in the hardware catalog.

SITOP PSU8600
The SITOP PSU8600 can be integrated in the hardware catalog of the TIA Portal V13 and higher via an HSP.
To install the latest version of the HSP 0103 V5.0 for the TIA Portal V13 you need a version that is at least higher than V13 SP1 UPD8.

 HardwareIntegration in the
hardware catalog
  Parameterizable devices
with firmware
 
 V13V14V15V13V14V15
Basic devices      

PSU8600 3ph 20A/4x5A PN
(6EP3436-8MB00-2CY0)

HSP 0103
x1x1V1.1
V1.2

V1.1
V1.22
V1.32

V1.1
V1.2
V1.3

 - HSP 0103--V1.4 -
PSU8600 3ph 40A/4x10A PN
(6EP3437-8MB00-2CY0)
HSP 0103
x1x1V1.0
V1.1
V1.2

V1.0
V1.1
V1.22
V1.32

V1.0
V1.1
V1.2
V1.3
 -HSP 0103--V1.4-
PSU8600 3ph 20A PN
(6EP3436-8SB00-2AY0)
HSP 0103
x1x1V1.1
V1.2

V1.1
V1.22
V1.32

V1.1
V1.2
V1.3
 -HSP 0103--V1.4
PSU8600 3ph 40A PN
(6EP3437-8SB00-2AY0)
HSP 0103
x1x1V1.1
V1.2

V1.1
V1.22
V1.32

V1.1
V1.2
V1.3

 -HSP 0103--V1.4-
Expansion modules      
CNX8600 4x5A
(6EP4436-8XB00-0CY0) 
HSP 0103
x1x1V1.0
V1.1
V1.2
V1.0
V1.1
V1.22
V1.32
V1.0
V1.1
V1.2
V1.3
 -HSP 0103--V1.4-

CNX8600 4x10A
(6EP4437-8XB00-0CY0)

HSP 0103
x1x1V1.0
V1.1
V1.2
V1.0
V1.1
V1.22
V1.32
V1.0
V1.1
V1.2
V1.3
 -HSP 0103--V1.4-

CNX8600 8x2,5A
(6EP4436-8XB00-0DY0)

-HSP 0103x1-V1.3V1.3
 -HSP 0103--V1.4-
Buffer modules   
 
BUF8600 100ms/40A
(6EP4297-8HB00-0XY0)
HSP 0103
x1 x1V1.0
V1.1
V1.2
V1.0
V1.1
V1.22
V1.0
V1.1
V1.2
V1.3
   HSP 0103  V1.4 
BUF8600 300ms/40A
(6EP4297-8HB10-0XY0)
HSP 0103
x1 x1V1.0
V1.1
V1.2
V1.0
V1.1
V1.22
V1.0
V1.1
V1.2
V1.3
 - HSP 0103--V1.4-
BUF8600 4s/40A
(6EP4293-8HB00-0XY0)
HSP 0103
x1 x1 V1.1
V1.2
V1.1
V1.22
V1.1
V1.2
V1.3
 - HSP 0103----
BUF8600 10s/40A
(6EP4295-8HB00-0XY0)
HSP 0103
x1 x1V1.1
V1.2
V1.1
V1.22
V1.1
V1.2
V1.3
 - HSP 0103-V1.4-
UPS module       
UPS8600
(6EP4197-8AB00-0XY0)
- HSP 0103--V1.4 -
Battery modules      
BAT8600 Pb
(6EP4145-8GB00-0XY0)
- HSP 0103--V1.4-

BAT8600 LiFePO4
(6EP4143-8JB00-0XY0)

- HSP 0103-- V1.4-

1 Integrated in the hardware catalog
2 With installation of SP1

SITOP  UPS1600
The SITOP UPS1600 can be integrated in the hardware catalog of the TIA Portal V12 and higher via an HSP.
To install the latest version of the HSP 0063 for the TIA Portal V12 you need a version that is at least higher than V12 SP1. For the TIA Portal V13 you need at least version V13 SP1 UPD8.

 HardwareIntegration in the
hardware catalog
  Parameterizable devices with firmware
 
  V12 V13V14 V15 V12 

 V13

V14  V15
Basic devices        
UPS1600 10A PN
(6EP4134-3AB00-2AY0)
HSP 0063
 HSP 0063
V6.0
 x1x1V1.14
V1.14
V1.22
V2.0
V2.1
V2.2
V1.14
V1.22
V2.0
V2.1
V2.22
V1.14
V1.22
V2.0
V2.1
V2.2
UPS1600 20A PN
(6EP4136-3AB00-2AY0)
 HSP 0063
HSP 0063
x1x1V1.14

V1.14
V1.22
V2.0
V2.1
V2.2

 V1.14
V1.22
V2.0
V2.1
V2.22
V1.14
V1.22
V2.0
V2.1
V2.2
UPS1600 40A PN
(6EP4137-3AB00-2AY0)
---HSP 0063
x1x1

---

V2.0
V2.1
V2.2
V2.0
V2.1
V2.22
V2.0
V2.1
V2.2
 Battery modules        
UPS1100 BATTERY MODULE 24 V/1.2 AH
(6EP4131-0GB00-0AY0)
HSP 0063
HSP 0063
x1x1V1.0V1.0V1.0V1.0 
UPS1100 BATTERY MODULE 24 V/2.5 AH
(6EP4132-0GB00-0AY0)
---HSP 0063
x1 x1---V1.0V1.0V1.0
UPS1100 BATTERY MODULE 24 V/3.2 AH
(6EP4133-0GB00-0AY0) 
HSP 0063
HSP 0063
x1 x1V1.0V1.0V1.0V1.0
UPS1100 BATTERY MODULE 24V/5AH LIFEPO
(6EP4133-0JB00-0AY0)
---HSP 0063
x1 x1---V1.0V1.0V1.0
UPS1100 BATTERY MODULE 24 V/7 AH
(6EP4134-0GB00-0AY0)
HSP 0063 HSP 0063
x1x1 V1.0V1.0V1.0V1.0
UPS1100 BATTERY MODULE 24 V/12 AH
(6EP4135-0GB00-0AY0)
---HSP 0063
x1x1 ---V1.0V1.0V1.0

1 Integrated in the hardware catalog
2 With installation of SP1


Further Information

  • Manual SITOP UPS1600 84977415
  • SITOP PSU8600 function and communication blocks 102379345 
  • SITOP UPS1600 function and communication blocks 78817848 


Additional Keywords

Power supply, Installation, HW Config, HW Update, Upgrade, HW, Hardware

Last Changes
Additions to the table for SITOP PSU8600: Integration of V1.4 in the TIA Portal and UPS1600 integration in TIA Portal V15.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.