×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109748099, Entry date: 09/18/2019
(8)
Rate

Testing and simulating HMI projects (TIA Portal) in conjunction with SIMATIC controllers, PLCSIM and PLCSIM Advanced

  • Entry
  • Associated product(s)
Plant-wide simulation of HMI project planning with WinCC TIA Portal in conjunction with hardware CPUs, PLCSIM and PLCSIM Advanced.

When developing an automation system, it is often necessary to test the planned software.
For this, however, various components may be required which are not yet available during the project planning phase. Depending on the scope of the task, several HMI operator interfaces and SIMATIC controllers may be required, for example.
So that these tests can still be carried out, it is recommended to simulate the required hardware.

The application example shows:

What options exist for testing and simulating the HMI configuration including the associated SIMATIC PLCs.
  • Simulation of one or more HMI projects
  • Simulation of one or more controllers

What the requirements are.
  • Installed software.
  • Required licenses.

Which settings need to be made.
  • In the HMI configuration.

  • On the configuration PC.

  • On the HMI operator panel.

The following figure shows the testing of a program where the hardware is partially present. The existing hardware communicates with the hardware simulated on the Field PG.



Documentation
  Simulation_of_WinCC_TIA_Portal_and_PLCs_en 

First publication
09/2019

Additional Keywords 
test, runtime simulation, PLCSIM Advanced V2.0, virtual machine, VM

_
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.