×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109748112, Entry date: 06/07/2017
(0)
Rate

Sales and delivery release for S7-SCL V5.6

  • Entry
  • Associated product(s)
The S7-SCL Version 5.6 has been released for delivery.

Operating systems

As of S7-SCL V5.6, the operating systems MS Windows 10 Pro and Enterprise, MS Windows Server 2012 as well as MS Windows Server 2016 are supported. For more detailed information on this, refer to the attached "Readme.rtf" file. Or click on the link below for the compatibility list.


Notes for S7-SCL V5.6 and STEP 7 V5.6

  • To ensure high security standards, our software is given a digital signature, among other things. This signature is checked by the operating system to detect any possible modifications made to the software from outside sources.

    If you are unable to install the product or an individual HSP, this may mean that the certificate stored in the operating system must be renewed. You can find more information on this at 109747789 

  • It is not longer possible to install S7 PDIAG V5.3 when using STEP 7 V5.6.

  • Please note that this is a new version of STEP 7. It is not possible to operate this product with licenses from the previous STEP 7 versions. This includes the current STEP 7 Professional V14 Combo licenses. Upgrade packages as well as PowerPacks are available with the release of STEP 7 Professional 2017.


Ordering data

The products with article numbers (order numbers) are listed in the attached file:.

  S7SCL_v5_6_orderlist.pdf (86,0 KB)


S7-SCL V5.6 Upgrade:

Customers using S7-SCL V5.3 can purchase an upgrade. The precondition for installation of the upgrade package is a valid license for S7-SCL V5.3.


Trial software download

Trial versions of the S7-SCL V5.6 can be downloaded and tested using this entry:109748118


Documents

  S7-SCL_-_Readme.rtf (261,5 KB)

  STEP_7_V56_-_Compatibility_list.pdf (433,9 KB)


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.