×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109748153, Entry date: 06/20/2017
(0)
Rate

Why does the WinCC Connection String Inspector in the AS Node Type Wizard of PCS 7/OPEN OS show an empty window?

  • Entry
  • Associated product(s)
Opening the WinCC Connection String Inspector in the AS Node Type Wizard shows an empty window, although there are connections defined in the WinCC project opened in the background.

This information is important for integrating 3rd Party Systems with PCS 7/OPEN OS V8.2 directly without OPC.
The proper connection string with the Initial Parameters cannot be retrieved.
  
For resolving this issue please install Microsoft SQL Server Native Client V10.0.
Direct download of the x64 version: 
http://go.microsoft.com/fwlink/?LinkID=188401&clcid=0x409.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.