×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109748188, Entry date: 06/12/2017
(0)
Rate

Process Historian 2014 SP2 Upd3 and Information Server 2014 SP2 Upd3

  • Entry
  • Associated product(s)
Update 3 is available for Process Historian 2014 SP2 and Information Server 2014 SP2.

What is new?
Update 3 for Process Historian 2014 SP2 and Information Server 2014 SP2 improves the behavior in several areas. For detailed information see the readme file.
  
Installation requirements
The installation of Update 3 for Process Historian 2014 SP2 and Information Server 2014 SP2 requires the installation of the following software:
    

  • Process Historian 2014 SP2 or Process Historian 2014 SP2 Upd1/Upd2

  • Inforrmation Server 2014 SP2 or Information Server 2014 SP2 Upd1/Upd2


The setup of Update 3 checks which Process Historian and Information Server components are installed on the target computer and updates them.

Readme files
Prior to installation read the notes and compatibility information in the readme files.
 Registrierung notwendig PH_IS_2014_SP2_Upd3_Readme.zip (505,8 KB)
  
Installation file
The following ZIP file includes the installation file.
 Registrierung notwendig PH_IS_2014_SP2_Upd3.zip (340,5 MB)
  
Note
Process Historian and Information Server can be used with SIMATIC PCS 7 and SIMATIC WinCC.
To keep your plant permanently up to date, refer to the information in the Compatibility Tool: 
www.siemens.com/kompatool.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit