×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109748192, Entry date: 06/13/2017
(2)
Rate

Sales and delivery release of V 4.1 of the ET 200SP interface module IM155-6PN in Standard function class (6ES7155-6AU01-0BN0)

  • Entry
  • Associated product(s)
The ET 200SP interface module IM155-6PN ST is available for delivery in a revised version, effective immediately. The new hardware has enabled the mains buffering time to be more than doubled to >= 10 ms.

The new interface module will be delivered with firmware V 4.1. In addition to lengthening the mains buffering time, the following optimizations have also been implemented with firmware V4.1:

  • Handling of user data qualifiers
  • Hot restart of stations connected to ET200AL modules via BA-Send after a fault occurs
  • Enhanced network scan ruggedness in conjunction with the PRONETA service tool in IRT mode


The V4.1 firmware also runs on the predecessor 6ES7155-6AU00-0BN0 interface module. In this case the mains buffering time remains the same.






The new IM155-6PN ST interface module market launch is a two-stage process.


Stage 1 (effective immediately)

Sales and delivery release of a BusAdapter (6ES7 155-6AA01-0BN0) bundle comprising:

  • IM 155-6 PN ST (6ES7155-6AU01-0BN0)
  • BusAdapter BA 2xRJ45 (6ES7193-6AR00-0AA0)
  • Server module (6ES7193-6PA00-0AA0)

The bundle with Article No. 6ES7155-6AA01-0BN0 is fully compatible with bundle 6ES7155-6AA00-0BN0. After sale of the predecessor bundles, all new orders will automatically be switched to the new version.


Stage 2 (2018)
Sales and delivery release of the interface module without a BusAdapter (6ES7 155-6AU01-0BN0), comprising:

  • IM 155-6 PN ST (6ES7155-6AU01-0BN0)
  • Server module (6ES7193-6PA00-0AA0)


Fully compatible with 6ES7155-6AU00-0BN0. After sale of the predecessor bundles, all new orders will automatically be switched to the new version.

Configuration can be carried out either via GSDML or HSP (STEP7 Classic and TIA Portal).



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.