×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109748210, Entry date: 07/07/2017
(2)
Rate

How do you use the function keys on the ITP1000 in WinCC Runtime Advanced?

  • Entry
  • Associated product(s)
In WinCC Runtime Advanced you can link system functions and scripts to a function key. The settings on the ITP1000 must be made in the IPC Configuration Center.

The example shows you how you can trigger a screen change with function key 1 of the ITP1000.

Procedure

  • Open IPC Configuration Center. Select the "Key definition" button. Click the "Key definition" button.


    Fig. 01
  • Assign Keycode F1 to the F1 key.



    Fig. 02
  • Open the TIA Portal.
  • Create a PC station.


    Fig. 03
  • Drag a WinCC RT Advanced into the PC station for visualization.


    Fig. 04
  • Create a new template in WinCC.


    Fig. 05
  • Open the template. Click the function key F1. Disable "Use global assignment".


    Fig. 06
  • Go to the "Events" of function key F1 and configure a screen change.


    Fig. 07
  • Link each screen with the template.



    Fig. 08
  • Download the project to your ITP1000.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.