×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109748224, Entry date: 06/26/2019
(6)
Rate

Digitalization with TIA Portal: Exchange of planning data from TIA Selection Tool via EPLAN Electric P8 in TIA Portal

  • Entry
  • Associated product(s)
TIA Selection Tool (TST) offers the possibility to export planning data (device configuration, network configuration) as “AutomationML” files. These AML files can be imported into EPLAN Electric P8. The planning data from EPLAN Electric P8 can also be exported to an AML file and imported into projects by TIA Portal.

The project planning data (device configuration, network configuration, PLC variables) of machines and systems are required by various tools. The open standard "Automation Markup Language" (AutomationML) has been developed so that project planning does not have to be recreated in each individual tool. AutomationML is an XML-based data format (AML file) for storing and exchanging project planning data.



To create an order list for the required components, the automation hardware is configured with the TIA Selection Tool (TST). TST enables direct ordering at the Siemens Industry Mall. TST can also be used to request the product data (EPLAN macros, dimensional drawings, 3D models, manuals, certificates, ...) of the Siemens articles used via the CAx Download Manager.

The configuration data generated in TST is exported to an AML file and imported into EPLAN Electric P8. The circuit diagrams are created in EPLAN Electric P8 using the imported data. For imported articles that are not available in the article management of EPLAN Electric P8, the EPLAN macros must be imported from the CAx Download Manager or macros from other manufacturers.

Once the circuit diagrams have been created, the data from EPLAN Electric P8 is exported to an AML file and imported into TIA Portal. The device configuration, the network configuration and the topology are adopted.

The following figure shows the workflow described in this application example.




Documentation and project example
  Documentation (1,5 MB)
 Registrierung notwendig  Project example (34,0 MB)


Further informationen
Application example: Integration of planning data from TIA Selection Tool to TIA Portal
TIA Selection Tool
EPLAN


Last changes
New workflow: TST -> EPLAN -> TIA Portal


Additional search terms

Digi Use Case, Digital Enterprise, Digital Workflow


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.