×
Siemens Industry Online Support
Siemens AG
Type de contribution : Exemple d’application ID de la contribution : 109748404, Date de la contribution : 05/10/2017
(3)
Évaluer

Using the SIMATIC ITP1000 in the Food and Beverage Industry

  • Contribution
  • Concerne le/les produits(s)
The SIMATIC ITP1000 opens the way to a new kind of mobile computing. Thus, in practice, it presents completely new fields for application with regard to communications, manufacturing or service. By means of various functions, this application example shows how to use the ITP1000 in your company.

The following functions are shown in the application example:

1. Logging on via RFID card
By logging on with an RFID card, you can realize a user administration.
This allows an access restriction to certain components of the plant.





2. Traceability of entries via WinCC Audit
You can use WinCC Audit to track operator actions in your production.



3. Reading codes (QR code, barcode, Data Matrix,...)
The SIMATIC ITP1000 supports a large number of different codes. You can use the integrated scanner to process these codes.

4. Communication via WLAN
Due to the interaction between an ITP1000 and a SCALANCE W access point, you are provided with a mobile operator panel that can be used for distributed plant structures such as in logistics.

5. Distributed plant operation
You can use the SIMATIC HMI HTTP protocol to enable data exchange between several operator panels. Thus, you have mobile access to production data via the ITP1000.

Documentation
  Documentation (3,9 MB)

Code
 Registrierung notwendig  Project for TIA V14 SP1 (96,1 MB)

Additional Keywords
Mobile Computing, tablet PC, codes, QR code, Data Matrix, barcode, card reader, camera



Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.
Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport