×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109748466, Entry date: 01/04/2018
(7)
Rate

How do you assign the associated PROFIsafe addresses to the F modules of the ET 200SP without additional Engineering?

  • Entry
  • Associated product(s)
In addition to assigning the PROFIsafe address for existing configurations, you also have the possibility of assigning via a user program.

Using the FB "PROFIsafeAddrAssign" provided here you can assign the PROFIsafe address for modules of the ET 200SP without additional Engineering. Using this block the memory card of the configuring and programming tool is written so that it is then also available for other controllers of a machine series.

 
Fig. 01: FB "PROFIsafeAddrAssign"

Apart from manual control of the FB "PROFIsafeAddrAssign" for assigning the PROFIsafe addresses, there is also an option for automatic address assignment. For this we provide the projects listed below (TIA Portal V14 und STEP 7 V5.5) that also include the possibility of configuration control. 

The associated documentation describes the necessary steps.  

The FB "PROFIsafeAddrAssign" is already in each of the projects. In addition, however, we also provide this separately in a block library.

Documentation
  Documentation (1,2 MB)

Automatic Address Assignment for S7-300 (With and Without Configuration Control)
TIA Portal V14 SP1:
 Registrierung notwendig  Project S7-300 (4,2 MB)

Automatic Address Assignment for S7-1500 (With and Without Configuration Control)
TIA Portal V14 SP1:
 Registrierung notwendig  Project S7-1500 (4,7 MB)

Block Library of the FB "PROFIsafeAddrAssign" for TIA Portal and STEP 7 V5.5
 Registration required  Block Library (631.0 KB)

Additional Keywords 
Option handling, F assignment, F address assignment 


 


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.