×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109748671, Entry date: 02/15/2018
(9)
Rate

Siemens Network Planner – SINETPLAN V1.0 SP1 Update 1 Download

  • Entry
  • Associated product(s)
Update 1 for SINETPLAN V1.0 SP1 is now available for download.


Download - SINETPLAN V1.0 SP1 Update 1 

As a registered customer, you can download the version for SINETPLAN V1.0 SP1 Update 1.

The new features are described in the delivery release for SINETPLAN V1.0 SP1 Update 1.   109748134 


>>> The new trial version for SINETPLAN V2.0 is available under the following link:   109763136 



Notes about downloading
The software is subjected to export restrictions. Download is only possible for registered users. Please note that, on account of the strong demand, the registration for export-restricted downloads will take some time.







Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit