×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109748679, Entry date: 11/09/2017
(0)
Rate

Restarting Windows at the SIMATIC S7-1500 Software Controller

  • Entry
  • Associated product(s)
A restart or an operating system crash of Windows does not affect the correct functioning of the CPU.

The CPU remains in the operating mode RUN and controls the automation process.
You can restart Windows using the following options:

  • Windows start menu
  • Windows command line
  • Restart using the TIA Portal instruction "SHUT_DOWN"
  • ODK function

If Windows crashes, you can restart Windows with the following configurations:

  • Configure Windows in such a way that it will be restarted automatically after a crash.
  • In the TIA Portal project, configure a block which queries the status of Windows and restarts Windows.


Figure 1

Downloads
  Documentation (1,6 MB)
”Registration TIA Portal V14 SP1 project (794.1 KB)
SHA-256 Checksum: BCCB57063F37B0A71E49F0B2309513CCA5ABD20EE51AAEEB8025A79E92657D34
 Registrierung notwendig  ODK project and batches (134,5 KB)
SHA-256 Checksum: 26F7B28C92AA8ACC58EF1ABA85B969B24975951EB0E360029F052193A8E03F95

You can find Informations to SHA-256 at the entry
How do you determine the SHA-256 checksum of a file?

Additional Keywords
Restart, reboot, WinAC


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.