×
Siemens Industry Online Support
Siemens AG
Entry type: Product note, Entry ID: 109748849, Entry date: 10/12/2017
(2)
Rate

Conversion: SIMATIC HMI COMFORT PANEL 15" - 22"

  • Entry
  • Associated product(s)
To ensure spare part supply, it was necessary to rework the SIMATIC HMI Comfort Panels 15" - 22". The updated and compatible devices - except for the Audio-In and the mini USB port - therefore are delivered with a new device image and new article numbers.

Conversion: SIMATIC HMI COMFORT PANEL 15" - 22"

Product name

Old article number

New article number

KP1500 Comfort

6AV2124-1QC02-0AX0

6AV2124-1QC02-0AX1

TP1500 Comfort

6AV2124-0QC02-0AX0

6AV2124-0QC02-0AX1

TP1900 Comfort

6AV2124-0UC02-0AX0

6AV2124-0UC02-0AX1

TP2200 Comfort

6AV2124-0XC02-0AX0

6AV2124-0XC02-0AX1


The products SIMATIC HMI KP1500 Comfort, TP1500 Comfort, TP1900 Comfort and TP2200 Comfort with article numbers ending in (-0AX0) will be phased out by October 1, 2017 and will still be available as spare parts, see also product life cycle SIMATIC HMI (91688124).

To ensure this comprehensive and long-term spare part service, the affected Comfort devices have been reworked and given new article numbers.

Important note:

The order and delivery of four successors ( *-0AX1) can most likely start of nov 2017.

The current devices ( *-0AX0) will still be available until 1 October 2018 as new parts. Discontinuation is scheduled for 1 October 2018, and it will not be possible to order new parts after that date. It is also possible that, depending on demand, the delivery of new parts may be limited between 1 October 2017 and 1 October 2018.

The successors have the following certificates at the start of delivery: CE, cULus, RCM (C-Tick), EAC as well as KCC.

The list prices of the successor devices are the same.

Engineering:
Existing projects must be upgraded with the engineering system WinCC V14 SP1 HSP and higher before they can be downloaded to the reworked devices.

The reworked Comfort Panels 15" - 22" can be configured as of SIMATIC WinCC V14 SP1 HSP and higher.

The project download takes place over PROFINET, PROFIBUS as well as USB file transfer. The mini USB port is not supported for the project transfer.

Bulk filling:
A "backup" of existing devices cannot be used as "Restore" on devices with new article number or vice versa (see Engineering). This applies to manual as well as automatic backup with SIMATIC HMI Memory Card.

Spare parts:
To replace defective devices, fully compatible replacement devices are still available in the spare part warehouse (EDN).

Starter kits
The starter kits are adapted to the successor devices (-0AX1) :

STARTER KIT

Order number

STARTER KIT TP1500 COMFORT

6AV2181-4QB00-0AX0

STARTER KIT TP1900 COMFORT

6AV2181-4UB00-0AX0

STARTER KIT KP1500 COMFORT

6AV2181-4QB10-0AX0

 


Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.