×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109749115, Entry date: 12/07/2018
(1)
Rate

Installing SIRIUS ACT coordinate switches in a SIRIUS ACT enclosure

  • Entry
  • Associated product(s)
This entry contains information on installing SIRIUS ACT coordinate switches in a SIRIUS ACT enclosure

QUESTION:

Can the SIRIUS ACT coordinate switches be installed in a standard SIRIUS ACT enclosure, e.g. 3SU1806-0AA00-0AB1, or only in the special enclosure, e.g. 3SU1801-1AA00-1AA1?

 

 

ANSWER:

The installation of 3SU1 coordinate switches with four-slot holders in a SIRIUS ACT enclosure (e.g. 3SU1806-0AA00-0AB1) is permitted under the following conditions:

  • The base plate must be removed
  • 3SU1 contact modules for front panel mounting must be used

Installation is possible both in plastic and metal 3SU1 enclosures.
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.