×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109749130, Entry date: 01/16/2018
(0)
Rate

Ensuring degree of protection IP69K in the case of drilled holes with groove

  • Entry
  • Associated product(s)
This entry contains information on degree of protection IP69K in the case of drilled holes with groove.

QUESTION:

Is degree of protection IP69/IP69K still ensured when installing 3SU1 commanding devices in a panel with "Eaton hole", that is, with groove?

 


ANSWER:

When installing 3SU1 commanding devices, degree of protection IP69K is also ensured in the case of drilled holes with groove, in accordance with the specifications of IEC 60947-5-1 and with a diameter of 22.5 mm.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.