×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109749306, Entry date: 08/30/2017
(10)
Rate

How do you save time when creating the library file for the Plant Automation Accelerator (PAA) Excel import?

  • Entry
  • Associated product(s)
This entry includes a description of the export of signals and parameters in the Plant Automation Accelerator (PAA) and the generation of a library file with the Excel generator.

Function of the Excel generator
The PAA provides a standard query to list all the existing signals of the Control Module Types (CMTs).
The user has to enter this signal data manually into an Excel table. Here, a special structuring of the Excel table is required.

Through the two queries of this FAQ response you can choose to export all the signals or all the parameters and signals. The export is converted automatically into the required structure by the Excel generator.

Advantages

  • Time saving through automatic generation

  • Minimization of error sources

  • Parameters can be included in the automatic generation

  • Prepared query with optimized sorting

 
Instructions
  LibGenerator PAA Instructions (1,6 MB)

Excel Generator
Registration required LibGeneratorV5 (349.0 KB)

SHA-256 Hash Code:
B80D168AA8487655C8CC5B71AA3101CCF84852C06B266D3B6553E13C77D71D64

 
Further Information

More help and useful information about PAA and COMOS is available via the COMOS topic page:

This page gives you a quick overview of the all the important PAA and COMOS entries in Online Support like:

  • Application Examples
  • FAQs
  • Forum
  • Media Systems (Videos)
  • Manuals
  • Services
  • Support
  • Training

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.