×
Siemens Industry Online Support
Siemens AG
文档类型 应用与工具 文档编号 109749356, 文档发布日期 2017年11月9日
(5)
评估

Positioning to Print Marks with SINAMICS V90 and SIMATIC S7-1200 (TO)

  • 文档
  • 涉及产品
A sensor detects print marks on a band feed. The positions of these print marks are stored with a SIMATIC S7-1200 and are intended for positioning a SINAMICS V90.

The TIA Portal V14 enables the control of a SINAMICS V90 drive via the pulse/direction interface (PTO). For this purpose, the SINAMICS drive can be configured in a SIMATIC S7-1200 controller as technology object and can be operated using Motion Control instructions.



In this application example, a cutting device is implemented. For this, print marks on a band have to be detected and their position has to be stored as setpoint values for positioning the band. The band is positioned by means of a SINAMICS V90.

Documentation and Project 
  Documentation (1,8 MB)
 Registrierung notwendig  STEP 7 project for TIA Portal V14 SP1 (1,5 MB)


安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.