×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109749356, Entry date: 11/09/2017
(5)
Rate

Positioning to Print Marks with SINAMICS V90 and SIMATIC S7-1200 (TO)

  • Entry
  • Associated product(s)
A sensor detects print marks on a band feed. The positions of these print marks are stored with a SIMATIC S7-1200 and are intended for positioning a SINAMICS V90.

The TIA Portal V14 enables the control of a SINAMICS V90 drive via the pulse/direction interface (PTO). For this purpose, the SINAMICS drive can be configured in a SIMATIC S7-1200 controller as technology object and can be operated using Motion Control instructions.



In this application example, a cutting device is implemented. For this, print marks on a band have to be detected and their position has to be stored as setpoint values for positioning the band. The band is positioned by means of a SINAMICS V90.

Documentation and Project 
  Documentation (1,8 MB)
 Registrierung notwendig  STEP 7 project for TIA Portal V14 SP1 (1,5 MB)


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.