×
Siemens Industry Online Support
Siemens AG
Tipo di articolo: Download, ID articolo: 109749385, Data articolo: 22/08/2017
(16)
Valuta

SIMOTION SCOUT, SCOUT Stand-alone and SCOUT TIA V5.1 HF1

  • Articolo
  • Riguarda prodotto/i

General Information

Attached you can find the download files of the engineering systems SIMOTION SCOUT, SCOUT Stand-alone and SCOUT TIA V5.1.
For a permanent operation of the products a new license-key for V5.1 is required.
If the included CamTool V4.1 is additional installed in the environment, also therefore a new license-key is required.

Further information about V5.1 HF1 is available in the delivery release notice 109749349.

Three different installation packages are offered as download: 


Installation package

Designation

Directories

Content

Package 1

SCOUT

V5.1 + HF1

(complete setup)

VOL1
SCOUT V5.1 + HF1
Addon
CamTool
HSP..TM_Timer_...
InstData
SSP_...
SIMOTION complete setup
SCOUT V5.1 + HF1
200SP Timer DIDQ
SSPs for SINAMICS

VOL2

SCOUT V5.1 + HF1

Documentation

Documentation
Utilities_Applications
 
SIMOTION V5.1 Documentation
 

 

VOL3

SCOUT TIA V5.1 + HF1

ScoutTia
MigTool
 
SIMOTION complete setup
SCOUT TIA V5.1 + HF1
(incl. CamTool V4.1 + HF1)
SCOUT Migrations-Tool Plug-In V5.1 + HF1
 

Package 2:

SCOUT Stand-alone 

V5.1 + HF1

(complete setup)

 

VOL1
SCOUT Stand-alone
 

V5.1 + HF1

SC
Addon
CamTool
HSP..TM_Timer_...
InstData
SSP_...

SIMOTION complete setup
SCOUT Stand-alone V5.1 + HF1

VOL2

SCOUT Stand-alone
 V5.1 + HF1
Documentation

Documentation
Utilities_Applications
 
SIMOTION V5.1 Documentation

VOL3

SCOUT TIA V5.1 + HF1

ScoutTia
MigTool
 
SIMOTION complete setup
SCOUT TIA V5.1 + HF1
(incl. CamTool V4.1 + HF1)
SCOUT Migrations-Tool Plug-In V5.1 + HF1
 

Package 3:

SCOUT TIA

V5.1 + HF1

(TIA Portal Client-Setup)

SCOUT TIA V5.1 + HF1

ScoutTia
MigTool 

SIMOTION complete setup
SCOUT TIA V5.1 + HF1
(incl. CamTool V4.1 + HF1)
SCOUT Migrations-T
ool Plug-In V5.1 + HF1

 Requirements for the installation:

  • For SCOUT, SIMATIC STEP 7 V5.6 must be installed on the engineering computer. The SIMOTION SCOUT V5.1 HF1 is a complete installation of SCOUT.
  • For SCOUT TIA, TIA Portal Framework V14 SP1 must be installed on the engineering computer (SCOUT TIA is a TIA Portal client setup). We recommend that you use the latest update of TIA Portal V14 SP1.



Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Read_OSS file.
Special information for resellers:

The information and the license terms in the ReadMe_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  Read_OSS.zip (5,8 MB)

Availability of Source Code
Certain license conditions of third-party software components used in this product may require Siemens to provide you with the source code and additional information for such components. In most cases, Siemens provides this information on or with the device. In case Siemens is technically unable to do so, you may request a copy of this OSS source code against payment of shipping and handling charges. Please send your request to the address provided at the end of this section.

Siemens AG 
Digital Factory
Customer Services DF&PD
DF CS SD CCC TS
Gleiwitzer Str. 555
90475 Nuernberg, Germany
Internet: http://www.siemens.com/automation/support-request
Tel.: +49 911 895 7222
Email: support.automation@siemens.com
 


Notes on the installation packages

  • The installation packages are divided into multiple files. First download all the parts into the same folder and run the file with the .exe extension. Select the root-directory of one of your hard disks to extract the setup files. The parts are then joined up and you can execute the setup.
  • Important information:
    After starting the .exe, please ensure that the length of the selected extraction path is no longer than 32 characters. If that will be ignored, the extraction will be aborted with an error and the software can't be installed.
  • Information about SHA-256 you can find at ID 109483101


Installation package 1: SIMOTION SCOUT V5.1 HF1

 Registrierung notwendig  SCOUT_V5_1_0_1.exe (2,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.001 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.002 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.003 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.004 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.005 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.006 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.007 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.008 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.009 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.010 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.011 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.012 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.013 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.014 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_1_0_1.015 (413,4 MB)

 Registrierung notwendig  SHA-256_Scout_V5.1.01.txt (1,9 KB)

Installation package 2 : SIMOTION SCOUT Stand-alone V5.1 HF1

 Registrierung notwendig  SCOUT_SA_V5_1_0_1.exe (2,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.001 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.002 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.003 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.004 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.005 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.006 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.007 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.008 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.009 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.010 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.011 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.012 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.013 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.014 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.015 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.016 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_1_0_1.017 (284,4 MB)

  SHA-256_Scout_SA_V5.1.01.txt (2,1 KB)


Installation package 3: SIMOTION SCOUT TIA V5.1 HF1

 Registrierung notwendig  SCOUT_TIA_V5_1_0_1.exe (2,6 MB) 
 Registrierung notwendig  SCOUT_TIA_V5_1_0_1.001 (667,6 MB) 
 Registrierung notwendig  SCOUT_TIA_V5_1_0_1.002 (667,6 MB) 
 Registrierung notwendig  SCOUT_TIA_V5_1_0_1.003 (667,6 MB) 
 Registrierung notwendig  SCOUT_TIA_V5_1_0_1.004 (251,6 MB) 

  SHA-256_Scout_TIA_V5.1.01.txt (1 KB)


Further downloads

The following downloads are also available as a single download from the Internet Product Support pages. The components are also includes in the download of SIMOTION SCOUT and SCOUT Stand-alone (= installation package 1 and 2).

  • SIMOTION C kernel/firmware V5.1 HF1 , see 31263919 
  • SIMOTION D kernel/firmware V5.1 HF1 , see 31045047 
  • SIMOTION  Firmware Support Package (FWSP) for device update tool, see 33119786 
Avvertenze di sicurezza
Al fine di proteggere impianti, sistemi, macchine e reti da minacce cibernetiche, è necessario implementare – e mantenere continuamente – un concetto di Industrial Security globale e all’avanguardia. I prodotti e le soluzioni Siemens costituiscono soltanto una componente imprescindibile di questo concetto. Ulteriori informazioni inerenti Industrial Security sono disponibili al sito
http://www.siemens.com/industrialsecurity.
Sostegno per la statistica
Con questa funzione gli ID del risultato di ricerca saranno visualizzati secondo il numero desiderato (formato .txt)

Generare elenco
Copiare URL
Visualizzzare questa pagina nel nuovo design
Cockpit mySupport