×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109749508, Entry date: 04/13/2021
(43)
Rate

Library of Basic Processes (LBP) for TIA Portal V16 (STEP 7 Basic / Professional, WinCC Comfort / Professional, WinCC Runtime Advanced / Professional), WinCC V7.5 SP2 and WinCC Open Architecture 3.17 with documentation, libraries and demo projects

  • Entry
  • Associated product(s)
Global library (TIA Portal) with 23 SCL function blocks for the control level and with faceplates for visualization with Comfort Panels, WinCC Runtime Advanced and WinCC Runtime Professional V16. Libraries for WinCC V7.5 SP2 and WinCC Open Architecture 3.17.

Plant manufacturers and system integrators are increasingly challenged to create more and more powerful automation solutions for achieving operational efficiency at ever lower costs.
At the same time, end customers demand improved process stability and plant availability without an increase in the engineering that is required.

The answer: Standardization.
With the TIA Portal, a very powerful and proven system platform is available, which is further enhanced with the Library of Basic Processes.


Fig. 1

The Library of Basic Processes (LBP) is a tested and design-oriented block library for the TIA Portal V15 (STEP 7 Basic / Professional, WinCC Comfort / Advanced, WinCC Runtime Advanced / Professional), WinCC V7.5 SP2 and WinCC Open Architecture 3.17.
With this library, you can solve a wide variety of automation tasks very efficiently and significantly reduce the engineering workload and thus the configuration costs as well as the project duration.

The library contains the following technological blocks:

  • Function blocks based on the Structured Control Language (SCL) for the control level

  • Faceplates and icons for the visualization level, scripts with Visual Basic Script

The following technological blocks are included:

  • LBP_Aggr8 – Control of up to 8 aggregates

  • LBP_AnaAvg – Average calculation with plausibility check

  • LBP_AnaRead - Analog value processing

  • LBP_ClctVal – Group display (without WinCC display)

  • LBP_CntrA – Integrating counter

  • LBP_CntrD – Difference counter

  • LBP_CntrP – Pulse counter

  • LBP_CtrlPID – Continuous PID controller

  • LBP_CtrlStp – Step controller

  • LBP_Intlk8 – Interlock for up to 8 signals

  • LBP_Msg8 – Message block for 8 messages

  • LBP_Mtr – Simple motor

  • LBP_MtrDS – Motor with two speeds and two directions of rotation

  • LBP_MtrF – Speed-controlled motor

  • LBP_OpAna – Switching analog values

  • LBP_OpDig – Switching a digital signal

  • LBP_Polygon – Conversion of values over 8 interpolation points

  • LBP_Select – Selection of values

  • LBP_SetCrv – Time-dependent setpoint curve

  • LBP_TimeSw – Time switch

  • LBP_Vlv – Simple valve

  • LBP_VlvA – Analog controlled valve

  • LBP_3wVlv – Three-way valve

  • LBP_SimoDir - Simple motor, controlled via SIMOCODE

  • LBP_SimoRev - Motor with two speeds and two directions of rotation, controlled via SIMOCODE

  • LBP_Sina - Motor, speed-controlled via G120

  • LBP_SinaExt - Motor, speed-controlled via G120X with commissioning option via HMI

Download documentation

Download libraries and demo projects

TIA Portal V16 (STEP 7 Basic / Professional, WinCC Comfort / Advanced / Professional, Comfort Panels, WinCC Runtime Advanced / Professional)

WinCC V7.5 (as of SP2)

WinCC Open Architecture 3.17

Note: You can receive the LBP for WinCC OA V3.16 from your Siemens contact partner

SITRAIN courses
Know-how for the products used in this application example is imparted in the following SITRAIN courses.

  • Programming basics
  • Basics of WinCC (TIA Portal) and WinCC V7
  

Additional information 

  • Application example "Demo projects for HMI Control Panels with WinCC V15/V15.1 (TIA Portal) for Basic Panels (2nd Generation), Comfort Panels and WinCC Runtime Advanced (TIA Portal)", Entry ID: 109757911
  • Demo project for WinCC Runtime Professional V15.1, Entry ID:109746940
  • Application example "Demo projects for SIMATIC WinCC V7.4 SP1", Entry ID: 109482515
  • FAQ "Where can you find more information about SIMATIC WinCC Open Architecture (formerly PVSS)", Entry ID: 45635235


Last change
New version V2.5, release for the TIA Portal V16 (STEP 7 Basic / Professional, WinCC Comfort / Advanced, WinCC Runtime Advanced / Professional),
New version V2.2, release for the TIA Portal V15.1 (STEP 7 Basic / Professional, WinCC Comfort / Advanced, WinCC Runtime Advanced / Professional), WinCC V7.5 and WinCC Open Architecture 3.16

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.