×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109749681, Entry date: 08/14/2017
(0)
Rate

Sales and delivery release of inscription labels and label holders for the operator control of SIMATIC HMI PRO devices.

  • Entry
  • Associated product(s)
The portfolio of system components for SIMATIC HMI PRO devices has been extended by two labeling options for self-labeling.

Inscription labels for labeling by customer



View of an installed inscription label in an illuminated pushbutton

A total of 216 inscription labels is available for printing on the four sheets in A4 format. The inscription labels can be integrated in illuminated pushbuttons and indicator lights.
The label is inserted behind the lens assembly of the operator control.




View of inserting an inscription label in an illuminated pushbutton




The print template for the inscription labels is available for download at the following ID: 109746380


Label holders for labeling by customer



View of a label holder


The label holders are used for labeling standard operator controls, not for Emergency Stop buttons, of the SIMATIC HMI PRO devices. They are installed from the outside on the operator control. The inscription label is 16.05 mm x 26.3 mm in size and can also be glued to the Extension Unit.
The scope of delivery includes 12 label holders.



View of inserting a label holder in a keyswitch



The print template for the label holders is available for download at the following ID: 109746380


Ordering data:

Description

Article number

Inscription labels for labeling by customer

6AV7674-1LB30-0AA0

Label holders for labeling by customer

6AV7674-1LB20-0AA0






Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.