×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109749807, Entry date: 08/22/2017
(0)
Rate

SIMOTICS: Conversion of the motors with DRIVE-CLiQ interface to temperature sensor Pt1000

  • Entry
  • Associated product(s)
As already announced in 109478106, the KTY84-130 temperature sensors installed in the motors will be discontinued. Motors without DRIVE-CLiQ interface have already been converted. In this respect, separate publications have already been issued for the individual motor series.

All motors with DRIVE-CLiQ interface will be converted to the new Pt1000 temperature sensor with deliveries performed as from Oct. 1, 2017.

The conversion is visible by the modified revision number and the indication of the Pt1000 temperature sensor on the motor rating plate.

The functions remain unchanged for the user. This is ensured by the digital DRIVE-CLiQ interface. Specific software requirements are not required.

The following motor series are affected by this conversion to Pt1000, listed with the new revision number and affected encoder variants.

SIMOTICS S-1FK7 Generation 1, only SH28

  • Article number:
    1FK702x-5xxxx-x?xx
    ? = D, L, P, U, V


  • New revision number: RN 007

Note: On 1FK7 with metal rating plate (option Q31), the temperature sensor is not explicitly stated on the rating plate.

SIMOTICS S-1FK7 Generation 2

  • Article number:
    1FK7xxx-2xxxx-x?xx
    1FK7xxx-3xxxx-x?xx
    1FK7xxx-4xxxx-x?xx
    ? = B, C, D, F, K, L, P, Q, R, U


  • New revision number: RN 006

Note: On 1FK7 with metal rating plate (option Q31), the temperature sensor is not explicitly stated on the rating plate.

SIMOTICS S-1FG1

  • Article number:
    1FG1xxx-x?xxx-xxxx
    ? = Q, R, P, U


  • New revision number: RN 002

SIMOTICS S-1FT7

  • Article number:
    1FT7xxx-5xxxx-x?xx
    1FT7xxx-7xxxx-x?xx
    ? = D, F, B, C, K, L


  • New revision number: RN 006

Note: On 1FT7, the temperature sensor is not explicitly stated on the rating plate.

SIMOTICS M-1PH8

  • Article number:
    1PH8xxx-x?xxx-xxx1
    ? = D, F, S, U


  • New revision number: RN 006 (only applies to SH80-160)

Note: On 1PH8 SH180-280, no revision number is specified on the rating plate. With 1PH8, the temperature sensor is always explicitly stated on the rating plate.

SIMOTICS T-1FW3

  • Article number:
    1FW3xxx-x?xxx-xxxx
    ? = D, F, P, U


  • New revision number: RN 002
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.