×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109750507, Entry date: 10/07/2020
(1)
Rate

SINAMICS firmware version 4.7 SP9 HF1 for the SINAMICS products G120 (CU230P-2, CU240B/E-2, CU250S-2), G120C, G120D (CU240D-2, CU250D-2), G110M and SIMATIC ET200pro FC-2

  • Entry
  • Associated product(s)
In this entry you will find the download as well as the ordering information for SINAMICS G120 multicard with version V4.7 SP9 HF1.

Important Note

The SINAMICS G120 Firmware Version 4.7 SP9 has achieved the milestone "Phase-out announcement" on 01.10.2019. With this background, we recommend using the latest SINAMICS G firmware. The milestone P.M410 "Product Cancellation" for V4.7 SP9 was also achieved on 01.10.2020.


For the latest firmware version please refer to the article 67364620 


Content of the SINAMICS G120 multicard V4.7 SP9 HF1

In this entry you will find the download as well as the ordering information for SINAMICS G120 multicard with version V4.7 SP9 HF1. The associated sales information is available under the following entry ID 109750805.

The SINAMICS G120 multicard contains the firmware releases for the following G120 products:

 

 SINAMICS family
Product 
Firmware (FW) version 
Internal firmware identifier 
G120PCU230P-2V4.7 SP9 HF1V04.71.04.01
G120

CU240B-2

CU240E-2

CU240E-2 F

CU250S-2

V4.7 SP9 HF1V04.71.04.01
G120CG120CV4.7 SP9 HF1V04.71.04.01
G120DCU240D-2
CU250D-2 
V4.7 SP9 HF1V04.71.04.01
G110MCU240M V4.7 SP9 HF1V04.71.04.01
ET 200pro FC-2ET 200pro FC-2V4.7 SP9 HF1V04.71.04.01

 

The installed firmware version can be read out at the SINAMICS G module using the parameter r0018 (internal version) or r0964 (completed device identification).

 

Note:
With this download, you can only upgrade SINAMICS products from the following firmware versions to V4.7 SP9 HF1:

  • from firmware V4.5: CU240E-2, CU240B-2, CU240D-2, CU250D-2 and G120C
  • from firmware V4.6: CU230P-2, CU250S-2 and G110M
  • from firmware V4.7 SP3 HF1: ET 200pro FC-2; 

 

An overview of the available firmware releases for SINAMICS G can be is given in the following entry ID: 67364620 


Third-party software – license conditions and copyright notes

You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the file READ_OSS.HTM file.


Special note for resellers

The notes and the license conditions contained in the READ_OSS.HTM file must be passed on to the purchaser in order to avoid the reseller and purchaser from violating the licensing conditions.


Availability of the source code

Some license conditions of third-party software components used in this product may oblige us to provide you with the source text and further information for these components. You can find this information either directly on the product itself or with the product (e.g. on a storage medium, DVD). Should this not be possible due to technical reasons, Siemens will gladly send you this OSS source code; however, you will have to pay the handling costs. Please contact the address specified at the end of this section regarding this matter.


Siemens AG 

Digital Factory

Customer Services DF&PD

DF CS SD CCC TS

Gleiwitzer Strasse 555

90475 Nuremberg, Germany

Internet: http://www.siemens.com/automation/support-request 

Tel.: +49 911 895 7222

 

 Registrierung notwendig  READ_OSS.HTM (1.1 MB) 

  

Current list of general conditions of the SINAMICS G120 for firmware V4.7 SP9

 Registrierung notwendig  SINAMICS_V479_Restrictions.pdf (15,4 KB) 

 

Provision of the SINAMICS G120 multicard V4.7 SP9 HF1

The content of the SINAMICS G120 multicard described above can be downloaded here:


Note:
From version V4.7 HF3, the runtime SINAMICS G120 firmware is not subject to any export restrictions as the output frequency has been limited to 550 Hz.
It is not subject to the Iran embargo, and is not listed in the EC Dual Use regulation. (AL = N).
It is not a US product (ECCN = N).

Alternatively, the SINAMICS G120 multicard V4.7 SP9 HF1 (SD card) can be ordered using the following article number 
6SL3054-7TE00-2BA0 .


Instructions for upgrading the firmware of the SINAMICS G120:

When upgrading, please refer to the instructions given in the "Firmware upgrade" chapter in the operating instructions of the particular Control Unit.

As an example, you can find the firmware upgrade/downgrade instructions for the CU240E-2 here:

 Registrierung notwendig  FW_Upgrade_Downgrade_G120_CU240BE2_en.pdf (296,5 KB) 


Note:

The zip file must be saved unpacked to the SD card in the root directory. An SD memory card with a capacity of least 256 MB must be used. Memory cards with capacities larger than 2 GB are not supported. An empty SINAMICS SD-CARD 512 MB can be ordered using article number 6SL3054-4AG00-2AA0.


List of faults and alarms 


List of faults and alarms for CU230P-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120P in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120P product is concerned, no additional support can be provided here.


 Registrierung notwendig  alarmlist_g120_cu230p_v04710300_deu.xml (423.5 KB)

 Registrierung notwendig  alarmlist_g120_cu230p_v04710100_eng.xml (415.1 KB)

 Registrierung notwendig  alarmlist_g120_cu230p_v04710100_ita.xml (443.1 KB)

 Registrierung notwendig  alarmlist_g120_cu230p_v04710100_fra.xml (448.2 KB)

 Registrierung notwendig  alarmlist_g120_cu230p_v04710100_esp.xml (436.8 KB)

 Registrierung notwendig  alarmlist_g120_cu230p_v04710100_chs.xml (384.2 KB)

 Registrierung notwendig  alarmlist_g120_cu230p_v04710100_rus.xml (551.9 KB)

 

List of faults and alarms for the CU240B-2 and CU240E-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the G120 in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120 product is concerned, no additional support can be provided here.


 Registrierung notwendig  alarmlist_g120_cu240b_e_v04710300_deu.xml (608.6 KB)

 Registrierung notwendig  alarmlist_g120_cu240b_e_v04710100_eng.xml (598.0 KB)

 Registrierung notwendig  alarmlist_g120_cu240b_e_v04710100_ita.xml (634.5 KB)

 Registrierung notwendig  alarmlist_g120_cu240b_e_v04710100_fra.xml (646.8 KB)

 Registrierung notwendig  alarmlist_g120_cu240b_e_v04710100_esp.xml (627.8 KB)

 Registrierung notwendig  alarmlist_g120_cu240b_e_v04710100_chs.xml (551.3 KB)

 Registrierung notwendig  alarmlist_g120_cu240b_e_v04710100_rus.xml (799.1 KB)


List of faults and alarms for the CU240D-2 and CU250D-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120D in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120D product is concerned, no additional support can be provided here.


 Registrierung notwendig  alarmlist_g120d_v04710300_deu.xml (782.4 KB)

 Registrierung notwendig  alarmlist_g120d_v04710100_eng.xml (773.1 KB)

 Registrierung notwendig  alarmlist_g120d_v04710100_ita.xml (819.4 KB)

 Registrierung notwendig  alarmlist_g120d_v04710100_fra.xml (833.8 KB)

 Registrierung notwendig  alarmlist_g120d_v04710100_esp.xml (810.4 KB)

 Registrierung notwendig  alarmlist_g120d_v04710100_chs.xml (713.3 KB)

 Registrierung notwendig  alarmlist_g120d_v04710100_rus.xml (1.0 MB)

 

List of faults and alarms for CU250S-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120 in the "xml" format.  Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120 product is concerned, no additional support can be provided here.


 Registrierung notwendig  alarmlist_g120_cu250s_v04710300_deu.xml (1.2 MB)

 Registrierung notwendig  alarmlist_g120_cu250s_v04710100_eng.xml (1.2 MB)

 Registrierung notwendig  alarmlist_g120_cu250s_v04710100_ita.xml (1.3 MB)

 Registrierung notwendig  alarmlist_g120_cu250s_v04710100_fra.xml (1.3 MB)

 Registrierung notwendig  alarmlist_g120_cu250s_v04710100_esp.xml (1.3 MB)

 Registrierung notwendig  alarmlist_g120_cu250s_v04710100_chs.xml (1.1 MB)

 Registrierung notwendig  alarmlist_g120_cu250s_v04710100_rus.xml (1.6 MB)

 

List of faults and alarms of the G120C

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120C in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120C product is concerned, no additional support can be provided here.


 Registrierung notwendig  alarmlist_g120c_v04710300_deu.xml (475.9 KB)

 Registrierung notwendig  alarmlist_g120c_v04710100_eng.xml (467.5 KB)

 Registrierung notwendig  alarmlist_g120c_v04710100_ita.xml (497.9 KB)

 Registrierung notwendig  alarmlist_g120c_v04710100_fra.xml (506.8 KB)

 Registrierung notwendig  alarmlist_g120c_v04710100_esp.xml (492.2 KB)

 Registrierung notwendig  alarmlist_g120c_v04710100_chs.xml (429.4 KB)

 Registrierung notwendig  alarmlist_g120c_v04710100_rus.xml (628.8 KB)

 

List of faults and alarms of the G110M

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the G110M in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G110M product is concerned, no additional support can be provided here.


 Registrierung notwendig  alarmlist_G110M_v04710300_deu.xml (512.7 KB)

 Registrierung notwendig  alarmlist_G110M_v04710100_eng.xml (503.5 KB)

 Registrierung notwendig  alarmlist_G110M_v04710100_ita.xml (536.4 KB)

 Registrierung notwendig  alarmlist_G110M_v04710100_fra.xml (545.8 KB)

 Registrierung notwendig  alarmlist_G110M_v04710100_esp.xml (529.9 KB)

 Registrierung notwendig  alarmlist_G110M_v04710100_chs.xml (463.4 KB)

 Registrierung notwendig  alarmlist_G110M_v04710100_rus.xml (675.4 KB)

 

List of faults and alarms of the ET200pro FC-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text of the ET200pro FC-2 in the "xml" format. Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the ET200pro FC-2 product is concerned, no additional support can be provided here.


 Registrierung notwendig  alarmlist_et200pro_v04710300_deu.xml (528.5 KB)

 Registrierung notwendig  alarmlist_et200pro_v04710100_eng.xml (518.7 KB)

 Registrierung notwendig  alarmlist_et200pro_v04710100_ita.xml (552.5 KB)

 Registrierung notwendig  alarmlist_et200pro_v04710100_fra.xml (562.4 KB)

 Registrierung notwendig  alarmlist_et200pro_v04710100_esp.xml (545.9 KB)

 Registrierung notwendig  alarmlist_et200pro_v04710100_chs.xml (475.8 KB)

 Registrierung notwendig  alarmlist_et200pro_v04710100_rus.xml (701.7 KB)

 

GSD files for project integration into the PROFIBUS configuring tool

PROFIBUS GSD files can be downloaded in the following entries:

 

GSDML files for integrating projects into the PROFINET configuring tool

PROFINET GSDML files can be downloaded in the following entries:

 

EDS files for integrating projects into the CANopen configuring tool

The EDS files for integrating projects into the CANopen configuring tools can be downloaded from the following entry:  (see 48351511)

 

STARTER

Within the scope of firmware version V4.7 SP9 HF1, STARTER V4.5 SP1 (see 109740000) must be used with the SINAMICS Support Package (SSP). The SSP is available for download from the following entry ID: 109477753.


With SSP, new functional features in firmware V4.7 SP9 HF1 can be configured using STARTER.


As part of the revision and simplification of the commissioning wizards, the SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" were introduced with STARTER V4.4 SP1 and SINAMICS G firmware V4.7 SP3. For additional information on this subject please refer to entry 109480663 .

 

Startdrive

Within the scope of firmware version V4.7 SP9 HF1, Startdrive V14 SP1 (see 68034568) must be used with Support Package V4.7 SP9 (see 68034568).

Upon importing the support package into an existing Startdrive V14 SP1 installation, new functions in the firmware version V4.7 SP9 HFx can be used with Startdrive.


As part of the revision and simplification of the commissioning wizards, the SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" were introduced with Startdrive V13 SP1 and SINAMICS G firmware V4.7 SP3. For additional information on this subject please refer to entry 109480663.

 

IOP-2 / BOP-2

The IOP-2 operator panel with firmware version V2.1 supports the new functions offered in SINAMICS G firmware V4.7 SP9 HF1. A complete overview of the expanded functionality for IOP-2 V2.1 can be found in the sales and delivery release 109748340 . In order to upgrade an existing IOP-2, the entry also includes an IOP-2 firmware download.


The BOP-2 operator panel (Article No.: 6SL3255-0AA00-4CA1) is automatically updated when using firmware V4.7 SP9 HF1. 

 

As part of the revision and simplification of the commissioning wizards, the SINAMICS application classes "Standard Drive Control", "Dynamic Drive Control" and "Expert" were introduced with Startdrive V13 SP1 and SINAMICS G firmware V4.7 SP3. For additional information on this subject please refer to entry 109480663.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.