×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109750720, Entry date: 10/04/2017
(1)
Rate

Sales and Delivery Release: SIMATIC PCS 7 Industry Library V9.0

  • Entry
  • Associated product(s)
SIMATIC PCS 7 Industry Library V9.0 is available effective immediately. The SIMATIC PCS 7 Industry Library V9.0 offers specific blocks and faceplates for various processes and applications as an extension of the PCS 7 Advanced Process Library.

1. Use and Area of Application

The functions of the SIMATIC PCS 7 Industry Library V9.0 are executed in the style of the SIMATIC PCS 7 Advanced Process Library and seamlessly complement their standard functionality. Together, the two libraries enable harmonized overall solutions for specific control system tasks in many different industries, e.g.:

  • Chemicals
  • Pharmaceuticals
  • Water and waste water
  • Glass and solar energy
  • Oil and gas industry
  • Food and beverage industry
  • Minerals and mining
   

2. Product Information

The SIMATIC PCS 7 Industry Library V9.0 offers the following function:

  • Parameter block with variable number of values
  • Functions for monitoring and controlling loads
  • Voting block for up to 8 analog values
  • Equipment monitoring for up to 16 units
  • Hierarchical multi-control room operation
  • Analog monitoring of 8 freely selectable limits
  • Analog monitoring with additional binary limit monitoring
  • Time switch for up to 8 time intervals
  • Polyline with variable number of interpolation points
  • Setpoint encoder with a variable number of setpoints
  • Functions for building automation
  • Simulation blocks
  • Standardized connection to external APC applications
  • Jump distributor for up to 5 jump destinations
  • Multiway diverter
  • Voting block for up to 8 digital values (new with V9.0!)
  • Interlock block 4x3 for up to 8 input signals over up to 3 levels (new with V9.0!)
  • Interlock block 8x4 for up to 16 input signals over up to 4 levels (new with V9.0!)
  • Communication blocks for coordinated communication between highly available and not highly available controllers. (New with V9.0!)

Note
Installation of TIA Portal software and PCS 7 V9.0 on one station is not approved. This is the reason why elements for configuring the WINCC Comfort Panel are not included in the product package of SIMATIC PCS 7 Industry Library V9.0. The elements will be made available as soon as the installation of the TIA Portal software for PCS 7 V9.0 is approved.

You can find additional information in the section "What's New" of the readme for SIMATIC PCS 7 Industry Library V9.0 under entry ID 109747449


3. Design

The SIMATIC PCS 7 Industry Library V9.0 is divided internally into two sub-libraries that can be separately installed:

  • Industry Library for PCS 7
  • Industry Library for S7
       
          

4. SIMATIC PCS 7 Industry Library Licensing

The licensing of the SIMATIC PCS 7 Industry Library V9.0 consists of three licenses:

  • Engineering license per engineering station
  • AS Runtime license per AS
  • Upgrade from V8.x to V9.0 per project

The Engineering license allows engineering of the components contained in SIMATIC PCS 7 Industry Library V9.0. Any licenses required for the use of the "IL for S7" for SIMATIC WinCC or SIMATIC STEP 7 are not included and must be additionally purchased.

The AS Runtime license is required for each AS (S7-400(H), S7-300, IM151-8, AS RTX or S7-1500) on which the components of the SIMATIC PCS 7 Industry Library V9.0 are to be loaded.

The PCS 7 AS RT PO concept for technological blocks of the SIMATIC PCS 7 Industry Library V9.0 also applies within SIMATIC PCS 7 or STEP 7 Engineering. Refer to the block description in the manual to learn the required number PCS 7 AS RT PO per block instance.

The Upgrade license is for upgrading plants that use licenses of the PCS 7 Industry Library V8.0, V8.1 or V8.2. The Upgrade license must be ordered once per project and applies to all PCS 7 Industry Library licenses included in the project.

     

5. Product and Ordering Information for PCS 7 Industry Library V9.0

ProductAritkle number

SIMATIC PCS 7 Industry Library V9.0 Engineering License
for one engineering station
 
  
  

6DL5410-8AX58-0YA0
SIMATIC PCS 7 Industry Library V9.0 Engineering License 
for one engineering station combined with a Runtime license for one automation system
 
  
  
6DL5410-8AA58-0YA0
SIMATIC PCS 7 Industry Library V9.0 Runtime License 
for one automation system
 
  
  
6DL5410-8AA58-0XL1
SIMATIC PCS 7 Industry Library V9.0 Runtime License 
for 30 automation systems (not bound to project)
 
  
  
6DL5410-8AB58-0XL1

SIMATIC PCS 7 Industry Library V9.0 Upgrade from V8.x to V9.0

Valid for all ES and AS Runtime licenses of a project

6DL5410-8AA58-0YE0

  

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.