×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109750782, Entry date: 01/11/2018
(1)
Rate

How do you save the service data from the CPU in a file in STEP 7 (TIA Portal) and via the web server?

  • Entry
  • Associated product(s)
In addition to the contents of the diagnostics buffer the service data of the S7-300/S7-400/S7-1500/ET 200SP CPUs (including CPU 1516 Pro-2 PN) includes further information about the internal status of the CPU.

Description

If a problem occurs with your CPU that you cannot solve via the diagnostics buffer, you also have the option of reading out the service data of the CPU and sending this data to Customer Support. If the service data is requested in the course of a Service Request, you can save the data as follows:
  • The service data for the S7-1500 is stored in STEP 7 (TIA Portal) in a Dmp file with the following naming convention:
    • "<Article number> <Serial number> <Time stamp>.dmp"
    • Example: 6ES7 518-4FP00-0AB0 S C-F8SF08202015 20170928 134724.dmp
  • In STEP 7 V5.x you obtain two files for the S7-300/S7-400 with the endings ".txt" and "bin".

You can also change the file names. Then send the data to Technical Support.

Reading out service data in STEP 7 (TIA Portal)for the S7-1500 CPU

  1. To read out the service data of the S7-1500 CPU, in the project navigation you open the PLC station and double-click "Online & Diagnostics".
  2. Under "Online access" you click the "Online connection" button to switch to the Online view.
  3. Under "Functions" you open the "Save service data" dialog.
  4. Select the storage path for the Dmp file and click the "Save service data" button.


Fig. 1

Note
With the S7-1500 CPU you can also save the service data on the SIMATIC Memory Card. Further information is available in the STEP 7 (TIA Portal) manual under "Save Service Data (S7-1500)".

Reading out service data for the S7-1500 CPU via the web server

  1. Open the web browser and enter the following address in the address bar:
    https:/ /<CPU IP address>/save_service_data
    Example: https:/ /192.168.0.1/save_service_data
  2. Click the "Save ServiceData" button and save the service data in a path on your hard disk.
     

Fig. 2

Further information about reading out service data for the S7-1500 via the web server is available in the manual under "Read out/Save Service Data".

Reading out service data in STEP 7 V5.x for the S7-300/S7-400 CPU

  1. In the SIMATIC Manager you select the menu command "PLC > Display Accessible Nodes".
  2. In the "Accessible Nodes" window you mark the node. In this example this is the station "pn-io".
  3. Using the menu command "PLC > Save Service Data..." you can save the service data in a directory on your hard disk.
    Note
    To save the service data from the S7-300 in a file you need the firmware V2.8 or higher for your CPU.


Fig. 3

Further Information
You can also obtain the service data via the SIMATIC Automation Tool. Instructions for this are available in the manual under Downloading Service Data From CPUs.

Creation Environment
The screens in this FAQ response were created with STEP 7 (TIA Portal) V14 and STEP 7 V5.5.


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.