×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109750845, Entry date: 10/06/2017
(15)
Rate

Product information on the firmware update for LOGO! 8 FS:04 and FS:05

  • Entry
  • Associated product(s)
A firmware update is available for LOGO! 8 FS:04 and FS:05. The firmware update includes the following changes:

Change

LOGO! 8 FS:04

LOGO! 8 FS:05

Improved display of messages texts and operation using cursor and F-keys for LOGO! base units, LOGO!8 TDE and web server in continuous operation (> 50 days)

Change

Change

Improved online test mode for diagram and network mode

Change

--

Parameter change for ON delay via LOGO! TDE

Change

--

Support of WinCC simulation

Change

--

Optimized display of bar graphs in the Web server

Change

--

Automatic saving of parameter changes on the MSD card during operation

Change

--

Support of the configured start value for the software switch function with activated retentivity

Change

--

Improved copy protection when using MSD cards

Change

--

Reading of programs of older LOGO! 8 (FS:01 to FS:04) from a MSD card

Change

--

Improved function of F keys in the Web server in TDE form

Change

--

Optimized operating hours counter in case of power failure

Change

--

Simultaneous support of NTP server and client for synchronizing the time and date

Change

--

Improved security for the integrated web server

Change

--

Notes on upgrading the firmware in LOGO! 8:


  • The firmware update can only be performed with LOGO! 8 FS:04 or FS:05.

  • The voltage supply for the LOGO! may not be interrupted during the entire time of the update and must be within the permissible range for the LOGO! in use.

  • The firmware can only be upgraded using SD cards.

  • With LOGO! 8 FS:04, the user program in the LOGO! base unit is deleted and LOGO! 8 is set back to the factory state

  • For LOGO! 8 FS:05, the program located in LOGO! is not deleted by upgrading the firmware.

  • Check the firmware update program, function and settings.

Instructions for upgrading the firmware for LOGO!8 FS:04:


Please note that upgrading the firmware for LOGO! 8 FS:04 restores LOGO! to the factory state and deletes the user program and all settings.

  1. Perform the free update from V8.1 to V8.1.1 of LOGO! Soft Comfort.

  2. Download the firmware update and save it on the PC.

  3. Copy and back up program on the PC in LOGO! with LOGO! Soft Comfort V8.1.1.

  4. Transfer the firmware update file on the MSD card to the root directory. Changes to the file, for example, file names, are not supported and LOGO! cannot complete the update as a result.

  5. Switch off the voltage supply for LOGO!.

  6. Insert the MSD card with the firmware update in LOGO! and carefully insert the MSD card holder in LOGO!.

  7. Switch on the voltage supply for LOGO!. Make sure that the voltage supply of the LOGO! base unit is stable during the entire firmware update process and within the range described in the manual.

  8. After completing the procedure, check the firmware update in the LOGO! the base unit.

  9. Transfer the previously saved program back in LOGO! and make all necessary settings.

  10. Check the program, function and settings and adapt them if necessary.

Instructions for upgrading the firmware for LOGO!8 FS:05:


  1. Perform the free update from V8.1 to V8.1.1 of LOGO! Soft Comfort.

  2. Download the firmware update and save it on the PC.

  3. Copy and back up program on the PC.

  4. Transfer the firmware update file on the MSD card to the root directory. Changes to the file, for example, file names, are not supported and LOGO! cannot complete the update as a result.

  5. Switch off the voltage supply for LOGO!.

  6. Insert the MSD card with the firmware update in LOGO! and carefully insert the MSD card holder in LOGO!.

  7. Switch on the voltage supply for LOGO!. The update is started automatically. Make sure that the voltage supply of the LOGO! base unit is stable during the entire firmware update process and within the range described in the manual.

  8. After completing the procedure, check the firmware update in the LOGO! the base unit.

  9. If necessary, transfer the previously saved program back in LOGO!.

  10. Check the program, function and settings and adapt them if necessary.

Notes on upgrading the firmware in LOGO! 8:


  • The firmware update can only be performed with LOGO! 8 FS:04 or FS:05.

  • The voltage supply for the LOGO! may not be interrupted during the entire time of the update and must be within the permissible range for the LOGO! in use.

  • The firmware can only be upgraded using SD cards.

  • After the firmware update, LOGO! 8 FS:04 is reset to the factory state. The user program in the LOGO! base unit is deleted.

  • For LOGO! 8 FS:05, the program located in LOGO! is not deleted by upgrading the firmware.

  • Check the firmware update program, function and settings.

Link to free upgrade to version V8.1.1 of LOGO! Soft Comfort:

http://w3.siemens.com/mcms/programmable-logic-controller/en/logic-module-logo/demo-software/Pages/Default.aspx

Link for downloading the required files for the firmware update of LOGO! 8 FS:04 and FS:05:

Registrierung notwendig logo_fw_v1_81_03_up_bm.zip (352.4 KB)

SHA-256 checksum: Registrierung notwendig Firmware_Update_fr_LOGO_8_FS04_und_FS05.txt (1 KB)


Information on SHA-256 109483101

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.