×
Siemens Industry Online Support
Siemens AG
ID de la contribution : 109751049, Date de la contribution : 09/05/2018
(10)
Évaluer

SIMATIC Technology - Motion Control: Overview and Important Links

  • Contribution
This topic page gives you an overview of the essential documents, entries and links on the topic of Motion Control. The topic Motion Control contains every control task to the operation of drives and capturing position values with the help of position sensors.



The tasks treated here reaches from steering for individual axes up to the method of several coordinate axes.

The motion instructions are based on the international PLCopen standard, thereby providing users a flexible means of programming their motion application without special knowledge. Applications can be programmed in all standard programming languages of IEC 61131.


Motion ControlSignalprocessing/-outputPID Control


S7-1500(T)

Manuals

SIMATIC S7-1500 S7‑1500 Motion Control V4.0 in TIA Portal V15
SIMATIC S7-1500 S7-1500T Motion Control V4.0 in TIA Portal V15
SIMATIC S7-1500 S7-1500T Kinematics Functions V4.0 in TIA Portal V15
SIMATIC S7-1500 S7-1500 Motion Control V3.0 in the TIA Portal V14
SIMATIC S7-1500 S7-1500 Motion Control V13 Update 3
Programming Guideline for S7-1200/S7-1500
Programming Styleguide for S7-1200/1500
Getting Started SIMATIC S7-1500


FAQs
What are the advantages of using the data type DB_ANY with Motion Control applications?
S7-1500T: Set synchronization in simulation - Retain a synchronized connection when locking the slave axis, for example
Camming with "MC_CamIn" in the S7-1500T
How to you operate the SINAMICS S120 drive via a Technology object (TO) on a SIMATIC S7-1500?
With Motion Control, how do you diagnose the configuration error if you do not get any valid encoder values with the modules TM PosInput and TM Count?
With S7-1200/S7-1500, how do you measure the total cycle time of an organization block?
Which organization blocks can you use in STEP 7 (TIA Portal)?
Compatibility Tool for Automation and Drive Technology
How can I locate the cause of a Motion Control Technology Alarm in a S7-1500 CPU ?
How Can You Integrate a Drive into the TIA Portal via the Device Master File (GSD)?
Automation Tasks in 10 minutes or less SIMATIC S7-1500: AT 8 - Integrated Positioning
Automation Tasks in 10 minutes or less SIMATIC S7-1500: AT 7 - Integrated Drives and Motion
How do you access the parameters of a drive which is controlled with the Motion Control function of an S7-1500 CPU?
Which IO controllers and IO devices support the following functions in STEP 7 (TIA Portal): IRT, prioritized startup, MRP, MRPD, PROFIenergy, Shared device, MSI/MSO, I device, clock-synchronized mode and option handling?
How do you control a KUKA robot with a SIMATIC controller?
Automation Tasks in 10 minutes or less - Drives and Motion
How do you program the automatic stop at the limit switches in jogging mode with S7-1500 Motion Control?
Isochronous mode with PROFINET - an example with SIMATIC S7-1500
With active referencing, why does the parameter for the approach direction not match the actual approach direction?
How can you realize the encoder configuration for the “positioning axis” technology object?
How do you configure the integrated counter of the compact CPUs 15xxC-1PN for Motion Control to make it usable for encoder acquisition?
How should you configure the encoder settings in the TO (Technology Object) for the SINAMICS V90 PN?
S7-1500(T): Manual determination of a compensation characteristic for hydraulic valves and hydraulic axes
How do you disable and enable the hardware limit switches of a Motion Control TO of an S7-1500 via the user program?
Why, in STEP 7 (TIA Portal), are no or only a few blocks displayed in the Task Card of the Motion Control instructions?
How do you control a DENSO robot with a SIMATIC controller?
How do you control a Stäubli robot with a SIMATIC controller?
Which requirements have to be fulfilled before a technology object can be enabled via "MC_Power"?
Which SINAMICS drives can you use with Motion Control and a SIMATIC S7-1500(T) controller?
Which controllers can you use for an actual value extrapolation?
Important settings when using Motion Control functions with an Open or Software Controller
How does a slave axis of camming behave during "Direct synchronous setting" (SyncProfileReference = 2)?

Application examples for "Motion Control"

SINAMICS G: Guide for Commissioning a Position-Controlled Drive
S7-1500T: Circular Motion on the Basis of Cam Disks "MoveCircle2D”
Using the MC-PreServo and MC-PostServo organization blocks
SIMATIC S7-1500: Cam Control Unit with time-based IO
SIMATIC S7-1500T Flying Saw
Diagnostics in User Program with S7-1500
Technology Objects of the SIMATIC S7-1500(T)
S7-1500T: Synchronizing in Standstill "LCISS_CamInStandStill" / "LCISSM_CamInStandStillMultiple"
Switchover and generation of cams with SIMATIC S7-1500T
Configuring Technology Objects with SIMATIC S7 1500 and SINAMICS S210 in TIA-Portal
Diagnostics Overview for SIMATIC S7-1200 and S7-1500
SIMATIC SimaHyd for hydraulic presses and applications

Application examples for "Drive Technology"

SINAMICS Blocks DriveLib for the control in the TIA Portal
SINAMICS G/S: Generating GSDML files for S120, S150, G130, G150, S110
SINAMICS G/S: Configuration of standard telegrams in TIA Portal
SINAMICS Positioning a G110M/G120 (Startdrive) with S7-1500 (TO) via PROFINET/PROFIBUS with Safety Integrated and HMI
SINAMICS G: Speed Control of a G110M / G120 (Startdrive) with S7-1500 (TO) via PROFINET or PROFIBUS with Safety Integrated (via Terminal) and HMI
SINAMICS G: Telegram Extension of a Position-Controlled Drive with SIMATIC S7-1500 (TO)
Configuring a SINAMICS S120 with Startdrive
SIMATIC/SINAMICS Getting started with SINAMICS V90 PN on S7-1500 Motion Control
Position Control of SINAMICS V90 with SIMATIC S7-1500 via IRT PROFINET
SIMATIC S7-1200/S7-1500 and SIMOTION: Acyclic Data Exchange
SIMATIC - Failsafe library LDrvSafe to control the Safety Integrated functions of the SINAMICS drive family


General application examples and libraries

SIMATIC S7-1500T Kinematics Transformation
SIMATIC S7-1500 / S7-1500T: Standard application axis control
SIMATIC/SIMOTION Library LCamHdl – Creation of cam disks at runtime
SIMATIC Library LPrintMark - Print Mark Acquisition with TO Measuring Input
SIMATIC Library LCalcMC – Calculation of motion profile details
SIMOTION, SIMATIC: Communication Library LCom for Ethernet Communication
Library of general functions (LGF) for SIMATIC STEP 7 (TIA Portal) and SIMATIC S7-1200 / S7-1500
Transforming warning and error messages of a SINAMICS drive with the aid of the XML parser and integrating them into a STEP 7 / HMI project
Controlling a KUKA Industrial Robot Using a SIMATIC S7-1500
The TIA Portal Tutorial Center (videos)
Guide to Standardization
SIMATIC S7-1500T Kinematics Computed Torque Control

 Branch solutions

Handling with SIMATIC S7-1500 T-CPU
SIMOTION/SIMATIC/SINAMICS - Converting Toolbox
SIMATIC/SIMOTION OMAC PackML V3 Machine and Unit States
SIMATIC/SIMOTION Weihenstephan Standards
SIMATIC S7-F/P Press Safety Blocks
SIMATIC/SIMOTION Intelligent Belt - Multi Belt Control
SIMATIC Winder and Tension Control
SIMATIC Simapress: Software package to automate a conventional flywheel press
SIMATIC S7-1500T Kinematics Control
SIMATIC S7-1500T Kinematics Manual Control
SIMATIC S7-1500T RotaryKnife
SIMATIC S7-1500T Kinematics Transformation
SIMATIC Traversing Drive


S7-1200

Manuals

SIMATIC STEP 7 S7-1200 Motion Control V6.0 in TIA Portal V15
SIMATIC STEP 7 S7-1200 Motion Control V6.0 in TIA Portal V14
SIMATIC STEP 7 S7-1200 Motion Control V13 SP1
Programming Guideline for S7-1200/S7-1500
Programming Styleguide for S7-1200/1500

 FAQs

How do you stop an axis with position accuracy in the case of product identification with the SIMATIC S7-1200?
What additions are included in the firmware changes of the S7-1200 controllers?
How Can You Integrate a Drive into the TIA Portal via the Device Master File (GSD)?
Automation Tasks in 10 minutes or less SIMATIC S7-1200: AT 7 - Simple Motion Commissioning
What additions are included in the firmware changes of the S7-1200 controllers?
Automation Tasks in 10 minutes or less - Drives and Motion
What are the advantages of using the data type DB_ANY with Motion Control applications?
With S7-1200/S7-1500, how do you measure the total cycle time of an organization block?

Application examples

S7-1200: Faceplate for Editing the "Command Table"
SIMOTION, SIMATIC: Communication Library LCom for Ethernet Communication
SIMATIC/SIMOTION OMAC PackML V3 Machine and Unit States
SIMATIC/SIMOTION Weihenstephan Standards
Diagnostics Overview for SIMATIC S7-1200 and S7-1500


S7-300(T)

Manuals

SIMATIC Engineering Tools S7 Technology
SIMATIC S7-300 CPU 31xT
SIMATIC S7-300 Connection of the SINAMICS S120 to the Technology CPU
SIMATIC S7 300 Automation Systems CPU 317T-2 DP: Controlling a SINAMICS S120
SIMATIC Automation System S7-300 CPU 317TF-2 DP: Controlling a SINAMICS S120 with Safety Functions

FAQs

How do you read the status of the digital inputs of the SINAMICS S120 CU320-2 in the user program of the controller part of a Technology CPU?
How do you read out the direction of rotation of an axis on a Technology CPU?
What do you do if a project with Technology CPU can no longer be opened in the S7T Config?
How do you configure for a Technology CPU a global measuring probe that is connected to the SINAMICS S120?
Which safety functions can you use with the interpolation on the fail-safe Technology CPU?
How can the interpolation point tables of the technology function FB 488 "MC_MovePath" be edited and administrated in the technology CPU via HMI Interface?
When do you use program simulation or axis simulation with a Technology CPU?
Why is the absolute value encoder adjustment lost after power-on of a Technology CPU?
How can I prevent error 13:76 and 3311 when compiling the technology of a Technology CPU?
Which MMC memory card do I need for the Technology CPUs?
How can a simple palletizer be realized with a technology CPU and the FB 488 "MC_MovePath"?
How can you replace the SINAMICS CU320 with the CU320-2 in a Technology CPU project with S7 Technology?
What options are there for reading hardware limit switch signals into a Technology CPU?
How do you avoid a STOP of the Technology CPU when stopping or interrupting a path object that is being moved by MC_MovePath (in S7 Technology V4.2)?
How do you interface and configure a 'SIMODRIVE sensor isochron' (synchronous PROFIBUS DP encoder) on Technology CPU?
How can I display a cam disk of the technology CPU on the HMI using WinCC flexible?
How must you parameterize the IM 174 in combination with the Technology CPU or SIMOTION when steppers are to be addressed without encoder feedback?
How can you read in an SSI absolute encoder into a Technology CPU if you do not use an IM 174 or an ADI4?
How can you replace the technology CPU already configured in a STEP 7 project with another technology CPU?
Technology CPUs: Which encoders can you use with the Technology CPUs?
Technology CPUs: How can you control a SINAMICS "Active Line Module" (ALM) via the PROFIBUS DP drive?
How can the SINAMICS S120 drive system be commissioned with the configuration tools of the technology CPU?
Error message ID 16#59A1 in the diagnostics buffer of Technology CPUs
Technology CPUs: How are the PROFIBUS, position control and interpolation cycles related?
Difference between the PROFIBUS DP interfaces on Technology CPUs
Why do the hydraulics function controller parameters on technology CPUs possess physical units which differ from the standard?
Technology-CPUs: Position Data
Technology CPUs: Determining a Technology Parameter Number
Technology CPUs: Release from a hardware limit switch
Technology CPUs: Diagnostics of an axis with Technology variables

Application examples

Technologie-CPU: Technology Template „MotionList Basic“
Technology CPUs: "Kinematics Simulation Center" - Connecting the Simulation Software to a Technology CPU Interface
Technology CPUs: "Drive Error Messages" Technology Template
Technology CPUs: Technology Template "Error Messages"
Technology CPUs: Technology Template "Hydraulics Characteristic"
Technologie CPUs: Technology Template "CrossCutter"
Technology CPUs: Flying shears with print-mark synchronization based on gear synchronism
Technology CPUs: Feeder for a press based on static cam disks
Technology CPUs: Technology Template "Flying shears"
Technology CPUs: Technology Template "Simple 3D-Interpolation with cam disks"
Technology CPUs: Technology Template "Move_Jog"
Technology CPUs: Palletizer with Simply Interpolating Axes Based on Cam Discs
Technology CPUs: Technology template “MoveCircle2D”
Technology CPU 317T-2 DP: Cross Slide / Single Belt Application
Technology CPUs: Parameterization of the "Gear Synchronization" Technology Function (SyncOp Guide)


Migration

Migration Guide: S7-31xT to S7-1500(T)



Further information

Information

SIMATIC Technology - The perfect basis for all technological tasks
SIMOTION at a glance
Interaction of SIMATIC control technology with SINAMICS drives

Training

SITRAIN - Training for Industry worldwide

Forum

SIMATIC Technology
SIMATIC S7-1500 - CPUs, peripherie, accessories
SIMATIC S7-1200 - CPUs, peripherie, accessories
SIMATIC S7-300 / S7-300F - CPUs, peripherie, accessories
STEP 7 Additional Software - S7-Technology, PID, Easy Motion Control
Drive Tools - SIZER, STARTER, Startdrive
SINAMICS


Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport
Liens connexes
    Pages thématiques concernant cette contribution