×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 109751358, Entry date: 02/14/2018
(1)
Rate

How do you migrate an AccessDB of the Plant Automation Accelerator (PAA) or COMOS to an SQL server?

  • Entry
  • Associated product(s)
The Plant Automation Accelerator (PAA) and COMOS can be operated with both an Access database and an SQL database. An Access database is suitable for testing and demonstration purposes. However, the size of the Access database is limited so an SQL database should be used for productive operations.

Important
For successful migration you first have to connect PAA or COMOS to an SQL server. Step-by-step instructions for this are available in the following FAQ response: 109751359.

Documentation
 How do you migrate an AccessDB of the Plant Automation Accelerator or COMOS to an SQL server? (1,3 MB)

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.