×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109751474, Entry date: 01/29/2018
(1)
Rate

SINAMICS S210 Firmware V5.1

  • Entry
  • Associated product(s)
Here you will find the SINAMICS S210 Firmware Version V5.1 for the 1AC 230 V converters.

 Description

The version description on the memory card (SD) is SINAMICS S210 V05.10.00.00.
The internal version number of the firmware is SINAMICS S210 V05.10.23.00.

When upgrading, please observe the instructions for the firmware update.

 Third-Party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the READ_OSS.HTM file.

Special information for resellers 

The information and the license terms in the READ_OSS.HTM file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

Availability of Source Code 

Certain license conditions of third-party software components used in this product may require Siemens to provide you with the source code and additional information for such components. In most cases, Siemens provides this information on or with the device (e.g. memory, DVD). In case Siemens is technically unable to do so, you may request a copy of of this OSS source code against payment of shipping and handling charges. Please send your request to the address provided at the end of this section.

Siemens AG
Digital Factory
Customer Services DF&PD
DF CS SD
Gleiwitzer Str. 555
90475 Nuernberg, Germany
http://www.siemens.com/automation/support-request
+49 (911) 895-7222
support.automation@siemens.com
Reference: Open Source Request (please specify product name and version, if applicable)

 Registrierung notwendig  Readme_OSS.htm (1,4 MB)

Restrictions of the SINAMICS S210

  SINAMICS_S210_Restrictions_V51.pdf (62,9 KB)

Instructions for the Firmware-Update of the SINAMICS S210 

  Firmware_Update_SINAMICS_S210_EN.pdf (820,2 KB)

 SINAMICS S210 Firmware Version V5.1 for 1AC 230 V converters

The following software can be downloaded:


Note
At present, the download version of the Runtime SINAMICS S210 Firmware Version V5.1 is not subject to any export restrictions because the output frequency has been limited to 550 Hz.
It is not subject to the Iran embargo, neither is it stated in the EC Dual Use Regulation. (AL = N).
It is not a US product (ECCN = N).

Alternatively, a new memory card (SD) with the following order number can be used:
Articel-No.: 6SL3054-4FB00-2BA0

 Lists of faults and alarms

The "alarmlist_*.xml" are not necessary for the correct operation of the firmware. They only contain a text-based export of the "Alarm messages" of the SINAMICS S210 in the "xml" format (this format guarantees a correct text-based representation, independent of the wide range of fonts that exist worldwide; this means that they can be converted error-free into other formats).
Customers occasionally request this exported text so that they can use it in their own applications or integrate it into external devices. As a consequence, as far as the SINAMICS S210 product is concerned, no additional support can be guaranteed here.

 Registrierung notwendig  Alarmlists_S210_V5_1.zip (1,0 MB)

 GSDML-Files for Integration into the PROFINET-Engineering tools

The PROFINET GSDML files are stored under the following path on the SINAMICS S210 CompactFlash card: 
   ..\SIEMENS\SINAMICS\DATA\CFG

They can also be downloaded here: (see109752524).

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Hinweis: Das Feedback bezieht sich immer auf den vorliegenden Beitrag. Ihre Nachricht wird an die Redakteure im Online Support gesendet. In einigen Tagen erhalten Sie von uns eine Antwort, wenn Ihr Feedback das erfordert. Ist für uns alles klar, werden wir Ihnen nicht mehr antworten.