×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109751614, Entry date: 12/20/2018
(2)
Rate

Burner Technology for S7 F Systems (Burner Library)

  • Entry
  • Associated product(s)
The application example Burner Technology for S7 F Systems (Burner library) supports you in the creation of Oil burner, Gas burner and Solid matter burner applications with single or multi burner.

In the process of creating a burner application several directives have to be complied. So the control logic is to be created according to specific functional requirements coming from EN 746-2. The functions of the library were developed with regards to individual sub‑functions, in order to ensure a modular application when using several burners. The function example follows the guidelines of EN 746-2 and further standards.

The library supports Oil burner, Gas burner and Solid matter burner as single and multi burner applications.
It has the following functions:

  • Function for controlling the ignition / pilot burner
  • Function for controlling the functions of a gas burner
  • Function for controlling the functions of an oil burner
  • Function for cleaning/blowing out the oil burner
  • Function to perform a tightness test of the gas valves
  • Function for controlling and monitoring of air dampers (and actuators with discrete position-feedback)
  • Function for controlling and monitoring of analogue actuators

The function blocks are prepared for realizing an electronic colligated solution. 

The following figure shows the technological layout of a burner system.



Validity
SIMATIC S7 F Systems V6.2

Download
 Registrierung notwendig  Documentation (2,1 MB)
 Download unterliegt Exportcontrolle  Burner Library (573,0 KB)

The Burner Library is subject to export restrictions. Before you can download the library, you must first authenticate yourself. To do this, click on the download link of the Burner Library and follow the instructions in the new window.

Further Versions
The Burner Library is also available for TIA Portal and Distributed Safety. You can find them in the following entries:

Maintaining the operational safety of your system
The operators of systems with safety-related characteristics must adhere to operational safety requirements. The supplier is also obliged to comply with special product monitoring measures. Siemens informs system operators in the form of personal notifications about product developments and properties which may be or become important issues in terms of operational safety. 

You should subscribe to the corresponding notifications in order to obtain the latest information and to allow you to make any necessary modifications to your system. 

Log in in the Industry Online Support. Here you find informations about individual notifications:
Useful functions in the Online Support (video)

Note
Dependent on the type of your burner, a system acceptance by impartial institution is possibly required. Whether your system is affected by this, you can see in the relevant directives / laws. A contacting of the institution is in either case advisable at an early stage