×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109751622, Entry date: 11/14/2017
(0)
Rate

Update 3 is available for SIMATIC S7-1500 Software Controller V2.1

  • Entry
  • Associated product(s)
Effective immediately, update 3 can be downloaded for all SIMATIC S7-1500 Software Controllers Version V2.1.

The following behavior has been revised with update 3:

  • When loading a PSC file, a reboot of the complete PC system is triggered during loading.
  • For command-controlled loading of a configuration ("PCSystem_Control /ImportConfig"), a load dialog of the PC station does not appear, and manual acknowledgment of the loading process is therefore no longer required.
  • The command "PCSystem_Control /GetStatus" can be executed with standard user rights.

The following behavior has been revised with update 3:

  • Import of a correct PSC file is no longer aborted with a timeout error message.
  • Import of a correct PSC file is no longer aborted with the error message "Component not registered" for the CPU or " Internal error" for the PC station.
  • The command "PCSystem_Control /PrintConfig <Filename>.psc /XML" returns a correct XML output.

Notes on installation

Procedure
1. Close the Software Controller and start the PC in "Windows" mode.
2. Copy the update onto your IPC.
3. Start the update by clicking on the downloaded file.
4. Carry out the individual installation steps.
5. Restart the PC once the installation is complete.

Availability

Update 3 is available for the following software controllers:

  • CPU 1505SP V2.1
  • CPU 1505SP F V2.1
  • CPU 1507S V2.1
  • CPU 1507S F V2.1

The updates can be downloaded from the following links:

109478528