×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109751779, Entry date: 11/09/2017
(3)
Rate

Sales and delivery release for SIMATIC HMI Comfort Panel 15" - 22"

  • Entry
  • Associated product(s)
As of November 08, 2017, the reworked versions of the SIMATIC HMI Comfort Panel 15" - 22" are available.

The devices have been reworked to ensure availability of spare parts. The updated and compatible devices - except for the Audio-In and the mini USB port - therefore are delivered with a new device image and new article numbers.



 Product name Old article number New article number
SIMATIC HMI KP1500 Comfort 6AV2124-1QC02-0AX0 6AV2124-1QC02-0AX1
SIMATIC HMI TP1500 Comfort 6AV2124-0QC02-0AX0 6AV2124-0QC02-0AX1
SIMATIC HMI TP1900 Comfort 6AV2124-0UC02-0AX0 6AV2124-0UC02-0AX1
SIMATIC HMI TP2200 Comfort 6AV2124-0XC02-0AX0 6AV2124-0XC02-0AX1

The functions of the devices are the same as those of the predecessor Panels. More details are available in the delivery release: 60456564

or in the Operating Instructions: 49313233

as well as in the Quick Installation Guide: 109750954


The successors have the following certificates at the start of delivery: CE, cULus, RCM (C-Tick), EAC as well as KCC.

The certificates for cULus Haz.Loc. and cFMus will be made available in the near future.

The list prices are identical to those of the old devices.

Configuration:
Configuration is performed with an HSP for WinCC in TIA Portal version V14 SP1 or in WinCC V15 and higher

Download V14 SP1 HSP for Comfort Panel 15" - 22":  72341852

Engineering:
Existing projects must be upgraded with the engineering system WinCC V14 SP1 HSP or WinCC V15 before they can be downloaded to the reworked devices.

The reworked Comfort Panels 15" - 22" can be configured as of SIMATIC WinCC V14 SP1 HSP or WinCC V15 

The project download takes place over PROFINET, PROFIBUS as well as USB file transfer. The mini USB port is not supported for the project transfer.

Bulk filling:
A "backup" of  existing devices cannot be used as "Restore" on devices with new article number  or vice versa (see Engineering). This applies  to manual as well as automatic backup with SIMATIC HMI Memory Card.

Spare parts:
To replace defective devices, fully compatible replacement devices are still available in the spare part warehouse (EDN).

Starter kits
The starter kits will be adapted to the successor devices (-0AX1) around the time these become available.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.