×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109752197, Entry date: 05/14/2020
(1)
Rate

Sales release of SINAMICS V20 multi-pump function

  • Entry
  • Associated product(s)
With immediate effect, the SINAMICS V20 multi pump function in firmware version V03.94.05.00 is released for sale.
The V20 multi pump function controls maximum 4 pumps with the I/O extension module. After the multi-pump control is enabled, you can configure the following four sub-functions: switching-in/-out, stop mode, pump switchover, and service mode.

Pump switch-in/switch-out



The inverter soft-starts the pumps one by one during switch-in sequence to achieve required system pressure. The inverter stages off the pumps one by one during switch-out sequence if the feedback pressure is higher than the required system pressure.

Stop mode

Two stop modes are available: Normal stop (all pumps in line system operation stop at the same time) and Sequence stop (all pumps in line system operation stop one by one).

Pump switchover

With pump switchover enabled, the Inverter monitors the operating status of all running pumps and manages pumps staging on/off according to continuous operating hours, in order to prolong the system lifetime.

Service mode

When a pump is in service mode, the inverter locks the corresponding relay, which allows you to perform troubleshooting of this pump without interrupting the operation of other pumps.

Enabling multi pump function

To enable this function, you must first download the multi-pump control script files to the inverter with the optional Parameter Loader and an SD card. Proceed through certain steps to download the script files into the inverter and apply.

Multi-pump control script file: 
 Registrierung notwendig  For V20 Firmware version V03.94.05.00 (6,5 KB)
 Registrierung notwendig  For V20 Firmware version V03.94.09.00 and above (5,9 KB)   

For detail steps, please refer to SINAMICS V20 Multi-pump Control Operating Manual:

  V20_multi_pump_op_man_0819_en-US-2020.pdf (3,4 MB)


Further information  

You can find further information here:siemens.com/sinamics-v20.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.