×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109752598, Entry date: 01/24/2018
(1)
Rate

SIMATIC ODK 1500S V2.5 Trial Download

  • Entry
  • Associated product(s)
SIMATIC ODK 1500S V2.5 is available as a 21-day trial version

As a registered customer, you can download the trial version for  SIMATIC ODK 1500S V2.5 and test it for 21 days. New features and changes as compared to earlier versions:

  • Development of C++ applications for the multifunctional platform CPU 1518(F)-4 PN/DP MFP
  • Development of function libraries for Windows with C# and Visual Basic
  • Support of the "Variant" data type with function libraries for Windows

You can find information about installation and the functions in the manual and product information:


Notes on version dependencies:

  • SIMATIC ODK 1500S V2.5 is installed alongside existing installations of previous versions, which means you can continue working with existing ODK applications.
  • To use the function libraries created with ODK 1500S V2.5, firmware version V2.5 for the S7-1500 Software Controller or CPU1518-4PN/DP MFP is required.

Notes about downloading:

The software is subject to export restrictions. Download is only possible for registered users. Please note that, due to strong demand, registration for export-restricted downloads will take some time.

SIMATIC ODK 1500S V2.5

 Download unterliegt Exportcontrolle  SIMATIC_ODK_1500S_V2_5.exe (1.9 GB)

 Registrierung notwendig  SIMATIC_ODK_1500S_V2_5.txt (1 KB)

Information on SHA-256  109483101

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.