×
Siemens Industry Online Support
Siemens AG
Type de contribution : Informations sur le produit ID de la contribution : 109753469, Date de la contribution : 20/04/2018
(2)
Évaluer

Sales and delivery release: SIRIUS Soft Starter ES V15 (TIA Portal)

  • Contribution
  • Concerne le/les produits(s)
Central software for configuration, commissioning, operation and diagnostics of SIRIUS 3RW44 soft starter.


The software and license key download versions of SOFT STARTER ES V15 have been released for delivery and are now available for download. Versions with software on DVD and license key on USB stick will be released until middle of May 2018. 
SOFT STARTER ES V15 is based on the central engineering framework Totally Integrated Automation Portal (TIA Portal) and can be seamlessly integrated when other TIA Portal-based software such as STEP 7 or WinCC is available, thus offering the user a uniform, efficient, and intuitive solution to all automation tasks. But those who use SOFT STARTER ES V15 as standalone software will benefit from its features.


Conversion to SOFT STARTER ES V15

The upgrade version to SOFT STARTERS V15 Standard or SOFT STARTER ES V15 Premium is of particular interest for users already using SOFT STARTER ES 2007, because it is offered a combo license. This combo license enables parallel use of SOFT STARTER ES 2007 and SOFT STARTER ES V15 (TIA Portal). In this way, users can familiarize themselves with the new software generation of SOFT STARTER ES based on the central engineering framework Totally Integrated Automation Portal (TIA Portal) and benefit from its advantages at the attractive price of an upgrade without dispensing with the tried and trusted version of SOFT STARTER ES 2007.

We highly recommend that new customers use SOFT STARTER ES V15, because only this version offers access to the full range of devices and features offered by 3RW44.


SOFT STARTER ES V15 (TIA Portal) offers the following features:

  • Easy configuration reduces the amount of engineering work and commissioning times
  • Detailed information, even about faults, helps maintenance personnel and shortens downtimes
  • Universally applicable through standalone version or seamless integration into the central engineering framework when other TIA Portal V15-based software such as STEP 7 or WinCC is available
  • Parameter changes are also possible during normal operation


What's new in SOFT STARTER ES V15?

The following innovations are available for SOFT STARTER ES in the TIA Portal:

  • SIRIUS Soft Starter ES V15 is available free of charge in the Basic version at the following link 109753470 
  • Customized configuration of device parameter display
    • A new view of the device parameters is available in the Parameter Editor. This view is called the Expert List.
    • Groups of parameters as well as individual parameters can be marked as favorites in the Expert List.
    • A filtered parameter view can be generated based on these favorites.
    • Export and import of this favorites selection (without values)
  • Mass Engineering   

    • A high-performance function for bulk engineering of devices within a project

    • Selected and appropriately set parameters can be transferred to a group of devices in a single step.

  • Automatic generation of PLC tags

    • If STEP 7 is also installed and a soft starter is linked to a PLC, PLC tags are automatically generated for all inputs and outputs communicated by means of a PLC via PROFIBUS or PROFINET.

    • The user can use this feature to directly access this data in the user program through symbolic addressing.


Three program versions

The user can choose between three different versions of SOFT STARTER ES.
These three versions are SOFT STARTER ES Basic, SOFT STARTER ES Standard and SOFT STARTER ES Premium.
New: SOFT STARTER ES Basic as of V15 is a high-performance tool for commissioning engineers or maintenance personnel. It is available for download free of charge in the Siemens Industry Online Support at the following link  109753470 

SOFT STARTER ES Standard and Premium with their extended range of functions are the perfect tools for engineers or project designers. Unlike the Standard version, SOFT STARTER ES Premium also permits configuration and diagnostics through PROFIBUS/PROFINET. Display of all operating, service and diagnostics data provides important information about the current state of the motor and plant at all times – everywhere on PROFIBUS or PROFINET.


Types of delivery and licenses

SOFT STARTER ES V15 is available as follows:

  • Floating license – the license per user
authorizes any one user – irrespective of the number of installations (unlike the single license, which can only be installed once). A license is only needed for the actual use of the program.

  • Combo license – license for parallel use
licenses parallel use of both the SOFT STARTER ES V15 Version and the version 2007

  • Trial license (free use of all program functions for 21 days for testing and evaluation, included on every product DVD, available in the download file of the SIRIUS ES program in the Service & Support portal).

The following types of delivery are also available:

  • Upgrade
    Switching from an old to a new version with expanded functions, e.g. upgrade from SOFT STARTER ES 2007 to SOFT STARTER ES V15, includes a combo license for parallel use of SOFT STARTER ES 2007 and SOFT STARTER ES V15
  • Software Update Service
    To keep you up to date at all times, we offer a special service that automatically supplies you with all service packs and upgrades for SOFT STARTER ES (TIA Portal). 


Replacement and compatibility

  • In addition to SOFT STARTER ES Version 2007, Version 15, based on the central engineering framework, Totally Integrated Automation Portal (TIA Portal), is available with immediate effect.
  • SOFT STARTER ES V15 is supplied as a combo license for parallel use of SOFT STARTER ES 2007 and SOFT STARTER ES V15.
  • Version 15 of SOFT STARTER ES (TIA Portal) is intended to replace SOFT STARTER ES V14.


  • License keys that were purchased for SOFT STARTER ES V14 can also be used for SOFT STARTER ES V15.
  • SOFT STARTER ES V15 (TIA Portal) is also intended to replace SOFT STARTER ES 2007.
  • SOFT STARTER ES V15 (TIA Portal) is compatible with software based on TIA Portal V15.
  • Parameter files that were created with SOFT STARTER ES 2007 can be migrated using the "Migrate project" function.
  • SOFT STARTER ES V15 (TIA Portal) supports all components of the 3RW44 soft starter.


Ordering data

SOFT STARTER ES V15 Basic
Software download Siemens Industry Online Support  109753470

SOFT STARTER ES V15 Standard
License key on USB stick, software on DVD                    3ZS1320-5CC11-0YA5  
License key download (OSD)                                           3ZS1320-5CE11-0YB5
Upgrade for SOFT STARTER ES 2007                            3ZS1320-5CC11-0YE5        

Software Update Service for 1 year                                  3ZS1320-5CC00-0YL5          

SOFT STARTER ES V15 Premium
License key on USB stick, software on DVD                    3ZS1320-6CC11-0YA5  
License key download (OSD)                                           3ZS1320-6CE11-0YB5          
Upgrade for SOFT STARTER ES 2007                            3ZS1320-6CC11-0YE5        

Software Update Service for 1 year                                  3ZS1320-6CC00-0YL5   


www.siemens.com/softstarter

Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.
Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport