×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109753687, Entry date: 01/19/2018
(0)
Rate

Information about SINAMICS DCC V3.1 SP1 HF2 for STARTER V5.1 SP1 and the firmware versions

  • Entry
  • Associated product(s)
The product version of SINAMICS DCC V3.1 SP1 HF2 for STARTER V5.1 SP1 has been released for delivery. In the following section, you will find additional information about SINAMICS DCC and product versions.

SINAMICS Drive Control Chart (DCC) is part of the Advanced Technology Function of SINAMICS S120. It consists of a graphic configuration tool (DCC editor based on SIMATIC CFC) and the function block libraries, also known as the Drive Control Block (DCB) libraries. Two types of DCB library are available, i.e. DCB Standard and DCB Extension. Comprehensive closed-loop control, arithmetic and logic blocks are available in the standard DCB libraries. On the other hand, using DCB Extension, customized block libraries can be created. You can find more information on SINAMICS DCB Extension at 74924161.

SINAMICS DCC is installed in addition to the STARTER engineering software. The SINAMICS DCC software package is a part of STARTER (DVD, software download), and is installed by selecting SIMATIC CFC during the setup. SINAMICS DCC supports subsequent installation of the software package. A (floating) engineering license is always required on each PC for configuring SINAMICS DCC. The license must be ordered separately with the SINAMICS DCC. When using blocks from the standard DCB libraries, which are listed in the SINAMICS DCC software package, a runtime license is not required.

SINAMICS DCC contains the SINAMICS DCC software package with SIMATIC CFC – and all the current DCB standard libraries on one data storage medium (DVD) and the engineering license (on a USB stick) for SINAMICS DCC based on the SIMATIC CFC version.

If the installation of SINAMICS DCC V3.1 SP1 HF2 is to take place in a STEP 7 environment – or in a PCS 7 environment with SIMATIC CFC for STEP 7 – please note that SIMATIC CFC in version V8.0, V8.0.4, V8.1, V8.2 or V9.0 must also be installed for STEP 7 and/or PCS 7.

Ordering data for the current version

New customers

For new SINAMICS DCC customers, the product version of SINAMICS DCC V3.1 SP1 HF2 – including full license (article number 6AU1810-1HA31-1XA0) – is recommended for SINAMICS MICROMASTER STARTER V5.1 SP1 109753725.

Content

  • DCC Editor based on SIMATIC CFC V8.2

  • Libraries: DCB standard libraries for the following firmware versions

    • SINAMICS V2.5 SP1

    • SINAMICS V2.6 SP1

    • SINAMICS V2.6 SP2

    • SINAMICS V4.3 SP1

    • SINAMICS V4.3 SP2

    • SINAMICS V4.4

    • SINAMICS V4.5

    • SINAMICS V4.6

    • SINAMICS V4.7

    • SINAMICS V4.8

    • SINAMICS V5.1

  • Engineering license: Full license for SIMATIC CFC V8.2 (not part of SINAMICS MICROMASTER STARTER DVD/download 26233208.

SINAMICS DCC can be used for training purposes for 14 days without the engineering license and without any restrictions. The SINAMICS DCC software package can be installed via the setup of SINAMICS MICROMASTER STARTER by selecting SIMATIC CFC during the setup. During configuration, a trial license (14 days) is activated.

Customers who are already using SINAMICS DCC

For customers who are already using SINAMICS DCC, the purchase of the product version, including upgrade license of SINAMICS DCC V3.1 SP1 HF2 (Article number 6AU1810-1HA31-1XE0) for SINAMICS MICROMASTER STARTER V5.1 SP1, depends on the existing SIMATIC CFC version.

Initial version Target version
SINAMICS DCC product version Existing SIMATIC CFC versionSTARTER V5.1 SP1 with SINAMICS DCC V3.1 SP1 HF2
V2.0 SPx V7.0Upgrade from SIMATIC CFC required*
V2.1 V7.0Upgrade from SIMATIC CFC required*
V7.1Upgrade from SIMATIC CFC required*

V2.2 SP1

67826366

V7.0Upgrade from SIMATIC CFC required*
V7.1Upgrade from SIMATIC CFC required* 
V8.0SIMATIC CFC can still be used

V2.3

98206100

V7.0Upgrade from SIMATIC CFC required*
V7.1Upgrade from SIMATIC CFC required*
V8.0SIMATIC CFC can still be used

V2.3 SP1

109477306

V7.0 Upgrade from SIMATIC CFC required*
V7.1Upgrade from SIMATIC CFC required*
V8.0 SIMATIC CFC can still be used
V8.1 SIMATIC CFC can still be used

V2.4 SP1

109740004

V7.0Upgrade from SIMATIC CFC required*

V7.1 

Upgrade from SIMATIC CFC required*
V8.0SIMATIC CFC can still be used
V8.1 SIMATIC CFC can still be used
V8.2SIMATIC CFC can still be used

* Upgrade to SIMATIC CFC V8.0 is required as a result of the minimum requirements of SINAMICS MICROMASTER STARTER V5.1 SP1 and SINAMICS DCC V3.1 SP1. We recommend upgrading to SIMATIC CFC V8.2 (Article number 6AU1810-1HA31-1XE0).

When using a 64-bit operating system, then as a minimum, SIMATIC CFC is V8.0 required. When changing over the operating system to 64 bit, we recommend an upgrade to SIMATIC CFC V8.2 (Article number 6AU1810-1HA31-1XE0).

Scope of delivery of SINAMICS DCC V3.1 SP1 HF2 upgrade license (Article number 6AU1810-1HA31-1XE0)

  • DCC Editor based on SIMATIC CFC V8.2

  • Libraries: DCB standard libraries for the following firmware versions

    • SINAMICS V2.5 SP1

    • SINAMICS V2.6 SP1

    • SINAMICS V2.6 SP2

    • SINAMICS V4.3 SP1

    • SINAMICS V4.3 SP2

    • SINAMICS V4.4

    • SINAMICS V4.5

    • SINAMICS V4.6

    • SINAMICS V4.7

    • SINAMICS V4.8

    • SINAMICS V5.1

  • Engineering license: Upgrade license for SIMATIC CFC V8.2 (not part of SINAMICS MICROMASTER STARTER DVD/download 26233208.

Supplementary conditions and functional restrictions

The supplementary conditions and functional restrictions of SINAMICS DCC V3.1 SP1 HF2 for SINAMICS MICROMASTER STARTER V5.1 SP1 and FW V5.1 can be taken from the readme file belonging to SINAMICS MICROMASTER STARTER V5.1 SP1 - or 109750851 .

For more detailed information, please contact your local Siemens Ansprechpartner 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.