×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109754628, Entry date: 07/15/2019
(1)
Rate

SIMATIC CFU Firmware

  • Entry
  • Associated product(s)
Firmware versions are available for SIMATIC CFU. It is recommended to upgrade to the current firmware version V1.1.2.

Procedure Firmware Update

  1. Carry out a FW update of the SIMATIC CFU PA to firmware version V1.1.x.
  2. Replace the configured SIMATIC CFU PA V1.0 in the HW configuration with the SIMATIC CFU PA V1.1 (object exchange).
    Select the SIMATIC CFU PA V1.0 and chose the option "Replace Object" in the context menu.
    Select the SIMATIC CFU PA V1.1 and confirm the exchange of the object.
  3. Open the SIMATIC PDM parameter list by double-clicking on the SIMATIC CFU.
    Important:
    Before downloading parameters to the SIMATIC CFU, you must upload the parameters (Upload to PG/PC).
  4. Save the loaded data in the project to save the current configuration of the SIMATIC CFU.


SIMATIC CFU Firmware V1.2.0 (current version – July 2019)

What´s new?

  • Support of additional bus adapters (2x VD, RJ45/LC, FC/LC)
  • Counter functionality / Frequency measurement 

Note
It is recommended to upgrade to the current firmware version V1.2.0

Installation file
The following zip file includes the installation file.

For STEP 7:
 Download unterliegt Exportcontrolle SIMATIC CFU Firmware-Version 1.2.0 (1,8 MB)

SHA256 Hash Code 1685DFA7E478580E187BAAC7D6C1318C0D81611AC90B1A68FC94142E2C373F38

For STEP 7 TIA Portal:
 Download unterliegt Exportcontrolle CFU UPD Package V1.2.0 (1,8 MB)

SHA256 Hash Code A455016B5B1C915B90907A43425580CCF9BD5EC89C6777024BA02F162428883A

Hardware Upgrade Package (HUP)
To configure SIMATIC CFU in SIMATIC PCS 7 you need the hardware upgrade package provided for download 109749915 

Product note
SIMATIC Compact Field Unit: 109749357 

Note
To keep your plant permanently up to date, refer to the information in the Compatibility Tool www.siemens.com/kompatool  


SIMATIC CFU Firmware V1.1.2 (backup – December 2018)

What´s new?

  • Optimization of automatic addressing
  • Improvement of stability 

Note
It is recommended to upgrade to the current firmware version V1.1.2.

Installation file
The following zip file includes the installation file.
 Download unterliegt Exportcontrolle  SIMATIC CFU Firmware-Version 1.1.2 (1,8 MB)

SHA256 Hash Code E205A8634BDB3D169325A5AB96755D4F7164914F5D49AC0505A10894D8BD4C36

Hardware Upgrade Package (HUP)
To configure SIMATIC CFU in SIMATIC PCS 7 you need the hardware upgrade package provided for download 109749915

Product note
SIMATIC Compact Field Unit: 109749357 

Note
To keep your plant permanently up to date, refer to the information in the Compatibility Tool www.siemens.com/kompatool 


SIMATIC CFU Firmware V1.1.1 (backup – October 2018)

What´s new?

  • Service interface
  • Manual field device integration
  • PROFINET certification

Installation file
The following zip file includes the installation file.

For STEP 7 from version 5.6 update 2:
 Download unterliegt Exportcontrolle  SIMATIC CFU firmware version 1.1.1 (1,8 MB)

SHA-256 Hash Code: CB297B7157BFA47E8DB7D53E0BB35BD1BAF854BA712E1FDC8FB2F1D3DFB5C4B3

For STEP 7 TIA Portal:
 Download unterliegt Exportcontrolle  CFU UPD Package V1.1.1 (1,8 MB)

SHA256 hash code: 7AFB09B208BEC8943FEBA66A3FFFD3F824720FC5FA7986FD1C73A7234E3613B6


SIMATIC CFU Firmware V1.0.1 (backup – January 2018)

What´s new?

  • Supports PROFIBUS PA field devices with PROFIsafe functionality
  • Increased robustness

System requirement
SIMATIC PCS 7 V9.0 SP1

Installation file
The following zip file includes the installation file.
 Download unterliegt Exportcontrolle  SIMATIC CFU firmware version 1.0.1 (1,7 MB)

SHA256 hash code: FA77899472EDF8D8242EC2BEAD6530FCCF8C1BA23194D30975E67A0AF6518BE2

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.