×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109755177, Entry date: 10/08/2018
(4)
Rate

Notes on Microsoft Updates 2018-01 (Meltdown and Spectre) with SIMATIC WinAC RTX

  • Entry
  • Associated product(s)
On January 3, 2018 and January 18, 2018, Microsoft released updates for its Windows operating systems to close the vulnerabilities which are grouped under the names Meltdown and Spectre.

SIMATIC WinAC RTX cannot be operated on PCs on which these updates have been installed. This especially applies to the following Microsoft updates:


Do not install these updateson PCs, on which SIMATIC WinAC RTX is operated, and do not install WinAC RTX on PCs, on which these KBs have already been installed.

This entry will be updated as soon as new information is available. Note: Updates which are declared as "Preview" are not installed or tested systematically.

You can find the latest information on the Microsoft Updates 2018-01 regarding Meltdown and Spectre and the operation with further SIMATIC software products in the product note 109754953 .


 


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.