×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109755181, Entry date: 01/22/2018
(0)
Rate

Delivery release for illuminated pushbutton (1 x NO contact and 1 x NC contact) for SIMATIC HMI PRO devices

  • Entry
  • Associated product(s)
The portfolio of system components for SIMATIC HMI PRO devices has been expanded by an illuminated pushbutton operator control (1 x NO contact and 1 x NC contact) for the Extension Unit.

The illuminated pushbutton (1 x NO contact and 1 x NC contact) is used to implement switch commands optionally as a NC contact and/or NO contact.

An operator control is supplied in a kit that contains the following components:

  • Operator control with threaded ring
  • Electronic connection module
  • Required fasteners
  • Lens cover (blue, red, green, yellow)


Representation of the illuminated pushbutton with lens covers
 



Illustration of installation of the illuminated pushbutton


Configuration:

The illuminated pushbutton can be immediately used for the hardwired versions of the Extension Unit.
Configuration of the PROFINET and PROFISAFE versions of the Extension Unit is performed using an HSP for TIA Portal V15.
You can find the HSP at the end of January with the following link:
Support Packages for the Hardware Catalog in the TIA Portal (HSP): 72341852

Ordering data:

Description

Article no.

ILLUMINATED PUSHBUTTON FOR EXT. UNIT (1S+1OE)

6AV7674-1MG00-0AA0

 



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.