×
Siemens Industry Online Support
Siemens AG
文档类型 产品通知 文档编号 109755189, 文档发布日期 2018年1月22日
(0)
评估

Change in supplier of external fans for SIMOTICS M-1PH8 main motors – shaft heights 180 and 225

  • 文档
  • 涉及产品
There has been a change in supplier of the single-phase EC external fans for the SIMOTICS M-1PH8 main motors in shaft heights 180 and 225 to ebmpapst. The new EC external fans are functionally equivalent and installation-compatible with the previous EC external fans from Ziehl-Abegg.

The change in external fans was concluded in December 2017 and is only valid for SIMOTICS M-1PH8 main motors in shaft heights 180 and 225.

The following SIMOTICS M-1PH8 main motors are affected by this change:

SIMOTICS M-1PH8 shaft height (SH)

11th position of the article number (for 1PH8)

180

0, 1 or 3, 4

225

0, 1 or 3, 4

The new external fan has new Article No. and Siemens No. designations on the rating plate, making a targeted approach possible.

SIMOTICS M-1PH8

External fan

Shaft height (SH)

Article number

Article No. designation

Siemens No. designation

180

1PH818x-xxx0x-xxxx

K3G250RR03H4

A5E37084747

1PH818x-xxx3x-xxxx

180

1PH818x-xxx1x-xxxx

K3G250RR17H9

A5E37084910

1PH818x-xxx4x-xxxx

225

1PH822x-xxx0x-xxxx

K3G280RR03H4

A5E37084871

1PH822x-xxx3x-xxxx

225

1PH822x-xxx1x-xxxx

K3G280RR04H9

A5E37084935

1PH822x-xxx4x-xxxx

The SIMOTICS M-1PH8 article number is not affected by this change.

Configuring and specification

Due to mechanical compatibility and the negligible difference in current consumption (see table), the existing sales documentation and configuration manual remain valid. The operating instructions,  109738144, have been updated and are available in electronic form . 
The dimensions and/or the dimensional disturbing contour of the motor are not changed by the new external fans.

The supply values for the new external fans are specified in the following table, but they can also be taken from the operating instructions:

SIMOTICS M-1PH8 article number

Current consumption (EC external fan)
at
200 V ... 277 V 1 AC/50 Hz, 60 Hz (± 10%) [A]

1PH818x-xxx0x-xxxx
1PH818x-xxx1x-xxxx
1PH818x-xxx3x-xxxx
1PH818x-xxx4x-xxxx


1.1 … 1.3

1PH822x-xxx0x-xxxx
1PH822x-xxx1x-xxxx
1PH822x-xxx3x-xxxx
1PH822x-xxx4x-xxxx


2.0 … 2.3

Note: For EC fans, the current drawn can briefly reach four times the specified current as a result of the electronic input circuitry.

安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.