×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109755199, Entry date: 01/23/2018
(0)
Rate

Sales and delivery release TeleControl Server Basic V3.1

  • Entry
  • Associated product(s)
Version 3.1 of the TeleControl Server Basic (TCSB) control center software is hereby released for sales and delivery. The software is scheduled for shipping ex warehouse starting at the end of January 2018. In addition to support for the SIMATIC RTU3010C, TCSB V3.1 offers functional enhancements and improvements.

1. Product description

The TeleControl Server Basic software connects up to 5,000 SIMATIC remote terminal units (RTUs) to a control center via mobile radio and Ethernet/Internet. Connection to the client takes place via OPC UA or OPC DA. This allows telecontrol solutions to be economically implemented in the fields of water/wastewater, logistics, maintenance and energy optimization.

The following enhancements and improvements are being released with TCSB V3.1:

 

1. Support for SIMATIC RTU3010C

The details for SIMATIC RTU3010C are available in the product tree of the SIMATIC RTU3000C product family:  https://support.industry.siemens.com/cs/ww/en/ps/21767/pm .

 

2. Data buffering at the OPC UA interface to prevent loss of data

If the connection between TCSB and OPC client is interrupted or if large amounts of data are to be transferred at once from the server to the client, the system was prone to loss of data in the past. This behavior has been corrected with V3.1: The process data can be buffered on the server and transferred to the client according to the update cycles set for the client. Data to be buffered is enabled with the Configuration and Monitoring Tool (CMT).

 

3. RTU3030C

The RTU3030C can now send a wake-up text message (SMS) that contains a specified date on which the RTU is to establish a connection to the TCSB. In addition, the connection mode "permanent" is supported for this station type.

 

4. Operation with SINEMA Remote Connect

To increase data security, the TCSB can be operated in combination with SINEMA Remote Connect. This means all telecontrol data is transferred between the RTUs and the control center over encrypted channels (VPN tunnel).

When using TCSB redundancy, we recommend you use a SCALANCE M/S upstream of the telecontrol server. In non-redundancy mode, this configuration as well as the configuration with a SINEMA Remote Connect client can be used.

 

5. Handling database import and database export

Handling has been made easier for exporting and importing the database. Both processes can now be handled via the CMT.

 

6. OPC UA: A value with "OnDataChange" and unchanged process value can now be transferred to the OPC UA client even if only the time stamp for this process value has changed and this process value has not been buffered.

 

7. For a GPRS connection to the RTU, the driver behavior for incompletely transferred telegrams has been optimized. In the past, this behavior could result in performance problems.

 

8. Advanced operating system release

Windows Server 2016 is also being released with TCSB V3.1.

 

This means the following operating systems have been released for TCSB V3.1:

  • Windows 10 Pro, Enterprise (64-bit)

  • Windows 8.1 Pro (64-bit)

  • Windows 7 Pro, Ultimate, Enterprise + SP1 (64-bit)

  • Windows Server 2016 Standard (64-bit)

  • Windows Server 2012 R2 Standard (64-bit)

  • Windows Server 2008 R2 Standard + SP1 (64-bit)

 

TCSB V3.1 has been tested with WinCC V7.3 and V7.4.

 

2. Ordering data

 

Product name

Order number

Standard licenses

 

TELECONTROL SERVER BASIC 8 V3.1

6NH9910-0AA31-0AA0

TELECONTROL SERVER BASIC 32 V3.1

6NH9910-0AA31-0AF0

TELECONTROL SERVER BASIC 64 V3.1

6NH9910-0AA31-0AB0

TELECONTROL SERVER BASIC 256 V3.1

6NH9910-0AA31-0AC0

TELECONTROL SERVER BASIC 1.000 V3.1

6NH9910-0AA31-0AD0

TELECONTROL SERVER BASIC 5.000 V3.1

6NH9910-0AA31-0AE0

Power packs for upgrading license scales

 

PP TELECONTROL SERVER BASIC 8 => 32 V3.1

6NH9910-0AA31-0AB1

PP TELECONTROL SERVER BASIC 32 => 64 V3.1

6NH9910-0AA31-0AF1

PP TELECONTROL SERVER BASIC 64 => 256 V3.1

6NH9910-0AA31-0AC1

PP TELECONTROL SERVER BASIC 256 => 1.000 V3.1

6NH9910-0AA31-0AD1

PP TELECONTROL SERVER BASIC 1.000 => 5.000 V3.1

6NH9910-0AA31-0AE1

Upgrade packages

 

TELECONTROL SERVER BASIC UPGR V3.1

Upgrade TCSB from V2 or V3.0 to V3.1

6NH9910-0AA31-0GA0

 

3. Miscellaneous

We offer an upgrade to V3.1 to owners of a TCSB V2 or V3.0 license: 6NH9910-0AA31-0GA0.

 

Security fixes and improvements

 

Previous versions:  

Sales and delivery release TeleControl Server Basic V3.0 + SP3:  109742130

Sales and delivery release TeleControl Server Basic V3.0 + SP2: 109483118

Sales and delivery release TeleControl Server Basic V3.0 + SP1: 109475218

Sales and delivery release TeleControl Server Basic V3: 94735146

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.