Entry type:
Product note
Entry ID:
109755213,
Entry date:
01/24/2018
Rate
SINAMICS Startdrive V14 SP1 Update 6
-
Entry
-
Associated product(s)
Update 6 for SINAMICS Startdrive V14 SP1 has been released for delivery
Update 6 for Startdrive V14 SP1 is available under 68034568 and includes improvements in the following areas:
- Drive commissioning in multi-user scenarios
- Stability of the control panel
- Stability when running on Windows 10.
Previous updates
The update is cumulative and contains all previous Startdrive V14 SP1 updates.
Installation instructions
The update can only be installed if Startdrive V14 SP1 has already been installed. After each installation of Startdrive V14 SP1, the update needs to be installed.
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Also available in the following languages:
- German
Entry belongs to product tree folder(s):
Rate entry
Feedback *)
Name
Phone number
email
DetailPages.Subject
Comment
Number of characters: 0 (max. 500)
Send copy of comment to sender. (login required)
*) Important: Please use this form for general feedback only. All technical and specialist topics should be directed to the expert community in the Technical Forum.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).
Copy URL
mySupport Cockpit
Product information