×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109755213, Entry date: 01/24/2018
(1)
Rate

SINAMICS Startdrive V14 SP1 Update 6

  • Entry
  • Associated product(s)
Update 6 for SINAMICS Startdrive V14 SP1 has been released for delivery

Update 6 for Startdrive V14 SP1 is available under 68034568 and includes improvements in the following areas:

  • Drive commissioning in multi-user scenarios
  • Stability of the control panel
  • Stability when running on Windows 10.

Previous updates

The update is cumulative and contains all previous Startdrive V14 SP1 updates.

Installation instructions

The update can only be installed if Startdrive V14 SP1 has already been installed. After each installation of Startdrive V14 SP1, the update needs to be installed.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit