×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 109755392, Entry date: 05/16/2018
(7)
Rate

SIMOTION SCOUT, SCOUT Stand-alone and SCOUT TIA V5.2 SP1

  • Entry
  • Associated product(s)

General Information

Attached you can find the download files of the engineering systems SIMOTION SCOUT, SCOUT Stand-alone and SCOUT TIA V5.2 SP1.
For a permanent operation of the products a new license-key for V5.2 SP1 is required.
If the included CamTool V4.2 SP1 is additional installed in the environment, also therefore no new license-key is required. CamTool V4.2 SP1 is still working with the license-key V4.1.

Further information about V5.2 SP1 is available in the delivery release notice 109755520.

Three different installation packages are offered as download: 

Installation package  Designation Directories Content
Package 1
SCOUT V5.2 + SP1
 VOL1
 SCOUT V5.2 + SP1
(several)

 AddOn
 CamTool
 HSP..TM_Timer_... 
 SSP_...
 SIMOTION complete setup SCOUT V5.2 SP1

 SIMOTION AddOn V5.2 SP1
 CamTool V4.2 SP1
 HSP for ET 200SP Timer DIDQ 
 SSPs for SINAMICS  
 

 VOL2
 SCOUT V5.2 + SP1
 Documentation
 Documentation
 Utilities_Applications 
 Dokumentation SCOUT V5.2 SP1
 Utilities & Applications V5.2 SP1
  VOL3
 SCOUT TIA V5.2 + SP1
 ScoutTia
 MigTool 
 SCOUT TIA V5.2 SP1 (incl. CamTool V4.2 SP1)
 SCOUT Migrations-Tool Plug-In  V5.2 SP1
 
 Installation package  Designation Directories Content
 Package 2
 
SCOUT Stand-alone
 V5.2 + SP1
 VOL1
 SCOUT Stand-alone 
 V5.2 + SP1
 (several)

 AddOn
 CamTool
 HSP..TM_Timer_... 
 SSP_...
 SIMOTION complete setup Stand-alone V5.2 SP1

 SIMOTION AddOn V5.2 SP1
 CamTool V4.2 SP1
 HSP for ET 200SP Timer DIDQ
 SSPs for SINAMICS 
  VOL2
 SCOUT V5.2 + SP1
 Documentation
 Documentation
 Utilities_Applications 
 Dokumentation SCOUT V5.2 SP1
 Utilities & Applications V5.2 SP1
  VOL3
 SCOUT TIA V5.2 + SP1
 ScoutTia
 MigTool 
 SCOUT TIA V5.1 SP1 (incl. CamTool V4.2 SP1)
 SCOUT Migrations-Tool Plug-In V5.2 SP1  
 Installation package   Designation Directories Content
 Package 3
 SCOUT TIA  V5.2+ SP1
(TIA Portal Client-Setup)
 SCOUT_TIA_V5_2_1_0
 ScoutTia
 MigTool 
  SCOUT TIA V5.2 SP1 (incl. CamTool V4.2 SP1)
  SCOUT Migrations-Tool Plug-In V5.2 SP1 

 

Requirements for the installation:

  • For SCOUT, SIMATIC STEP 7 V5.6 must be installed on the engineering computer. The SIMOTION SCOUT  V5.2 SP1 is a complete installation of SCOUT.
  • For SCOUT TIA, the TIA Portal Framework V15 must be installed on the engineering computer (SCOUT TIA is a TIA Portal client setup). We recommend that you use the latest update of TIA Portal V15.


Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the Read_OSS file.
Special information for resellers:

The information and the license terms in the ReadMe_OSS file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

 Registrierung notwendig  Read_OSS.zip (6,6 MB)

Availability of Source Code
Certain license conditions of third-party software components used in this product may require Siemens to provide you with the source code and additional information for such components. In most cases, Siemens provides this information on or with the device. In case Siemens is technically unable to do so, you may request a copy of this OSS source code against payment of shipping and handling charges. Please send your request to the address provided at the end of this section.

Siemens AG 
Digital Factory
Customer Services DF&PD
DF CS SD CCC TS
Gleiwitzer Str. 555
90475 Nuernberg, Germany
Internet: http://www.siemens.com/automation/support-request
Tel.: +49 911 895 7222
Email: support.automation@siemens.com
 


Notes on the installation packages

Important information

  • After starting the .exe, please ensure that the length of the selected extraction path is no longer than 32 characters. If that will be ignored, the extraction will be aborted with an error and the software can't be installed.
  • For SCOUT V5.2 SP1 in connection with STEP 7 V5.6 is the usage of HF3 for STEP 7 V5.6 recommended and released.
    STEP 7 V5.6 HF4 must not be used
    .

  • In SCOUT, SCOUT SA and SCOUT TIA V5.2 SP1 in the combination with Microsoft Office 64-Bit, it may be not possible any more to open SIMOTION projects. Please note therefore the FAQ,  Entry-ID 109476578 .

Additional information

  • The installation packages are divided into multiple files. First download all the parts into the same folder and run the file with the .exe extension. Select the root-directory of one of your hard disks to extract the setup files. The parts are then joined up and you can execute the setup.
  • Information about SHA-256 you can find at ID 109483101.


Installation package 1: SIMOTION SCOUT V5.2 SP1

 Registrierung notwendig  SCOUT_V5_2_1_0.exe (3,0 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.001 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.002 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.003 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.004 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.005 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.006 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.007 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.008 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.009 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.010 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.011 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.012 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.013 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.014 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.015 (667,6 MB)
 Registrierung notwendig  SCOUT_V5_2_1_0.016 (365,2 MB)

 Registrierung notwendig  SHA-256_SCOUT_V5_2_1_0.txt (2,4 KB)



Installation package 2: SIMOTION SCOUT Stand-alone V5.2 SP1

 Registrierung notwendig  SCOUT_SA_V5_2_1_0.exe (3,0 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.001 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.002 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.003 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.004 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.005 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.006 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.007 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.008 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.009 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.010 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.011 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.012 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.013 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.014 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.015 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.016 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.017 (667,6 MB)
 Registrierung notwendig  SCOUT_SA_V5_2_1_0.018 (236,3 MB)

 Registrierung notwendig  SHA-256_SCOUT_SA_V5_2_1_0.txt (2,6 KB)


Installation package 3: SIMOTION SCOUT TIA V5.2 SP1

 Registrierung notwendig  SCOUT_TIA_V5_2_1_0.exe (3,0 MB)
 Registrierung notwendig  SCOUT_TIA_V5_2_1_0.001 (667,6 MB)
 Registrierung notwendig  SCOUT_TIA_V5_2_1_0.002 (667,6 MB)
 Registrierung notwendig  SCOUT_TIA_V5_2_1_0.003 (667,6 MB)
 Registrierung notwendig  SCOUT_TIA_V5_2_1_0.004 (448,7 MB)

 Registrierung notwendig  SHA-256_SCOUT_TIA_V5_2_1_0.txt (1 KB)


Further downloads

The following downloads are also available as a single download from the Internet Product Support pages. The components are also includes in the download of SIMOTION SCOUT and SCOUT Stand-alone (= installation package 1 and 2).

  • SIMOTION C kernel/firmware V5.2 SP1, see 31263919 
  • SIMOTION D kernel/firmware V5.2 SP1, see 31045047 
  • SIMOTION  Firmware Support Package (FWSP) for device update tool, see 33119786 
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.