×
Siemens Industry Online Support
Siemens AG
Type de contribution : Informations sur le produit ID de la contribution : 109755520, Date de la contribution : 16/05/2018
(2)
Évaluer

Delivery Release of Motion Control System SIMOTION Version V5.2 SP1

  • Contribution
  • Concerne le/les produits(s)
Effective immediately, SIMOTION version V5.2 SP1 is released for delivery.

Actualiation (06/2018)
The delivery of the DVD products is now released too. Active Software Update Service (SUS) will get the DVDs automaticly,


1. General information

SIMOTION V5.2 SP1 is released for delivery effective immediately. The release refers to the following components:

  • SIMOTION SCOUT engineering system, SCOUT stand-alone and SCOUT TIA, version V5.2 SP1
  • SIMOTION Kernel/Firmware V5.2 SP1
  • DCC SIMOTION V3.2 SP1

SIMOTION V5.2 SP1 is the first generally released version within the major version V5.2.
The above-mentioned software components will initially be made available via Online Software Delivery (OSD) as well as the Industry Online Support International (SIOS) (see under downloads). As a consequence, the complete SCOUT environment and firmware V5.2 SP1 can be downloaded.
SCOUT V5.2 SP1 requires a new license key.
SIMOTION DCC V3.2 SP1 can also be used without restrictions with currently available DCC SIMOTION licenses that can still be ordered and installed with SCOUT (see section SIMOTION DCC).

 

2. Functional scope

Overview of new SIMOTION V5.2 SP1 functions

New functions are available with SIMOTION V5.2 SP1. The most important new functions are:

  • SIMOTION in the TIA Portal V15 with SCOUT TIA V5.2 SP1 
  • Optimizations for SCOUT and SCOUT TIA (e.g. in editors)      
  • SIMOTION D with SINAMICS Integrated V5.1 incl. new safety functions such as 
    • Safe Cam (SCA) / Telegram 903
    • Safely-Limited Acceleration (SLA)

  • RT Adaption SINAMICS S210 / Telegram 750


Detailed information about new SIMOTION V5.2 SP1 functions

A detailed description of the new functions is provided in the following documentation:

  Simotion_Neue_Funktionen_V521_DE.pdf (491,7 KB)

  Simotion_New_Features_V521_EN.pdf (491,1 KB)


3. Compatibility

Projects which were created with older versions can be upgraded to the new version (e.g. if the existing project is to be extended to include functions of version V5.2 SP1). A description is provided in the readme or in the manual.
 
Detailed information about combining software products is provided in the compatibility lists for SCOUT and SCOUT TIA on the Internet under 18857317.

You can also find a detailed, regularly updated list of the I/O modules released for SIMOTION as well as notes on their use on the Internet at 11886029

The SINAMICS STARTER commissioning tool, as well as SIMATIC S7 Technology (STEP 7 option for configuring the CPU 31XT-2 PN/DP), are integrated in SIMOTION SCOUT V5.2 SP1.


4. Test certificates

SINAMICS Safety Integrated functions are generally certified by independent institutes. You can request a list of currently certified components from your local Siemens office. For questions relating to certifications that still have not been completed, please contact your local Siemens representative.

Detailed information on the SINAMICS Integrated firmware version of SIMOTION D including the Safety versions is available in the entry 31045047 

The current status of the available certificates with regard to international standards and machine safety (TÜV, IFA) can be found at the following link:https://support.industry.siemens.com/cs/de/en/ps/14505/cert


5. Released components

SIMOTION SCOUT incl. SCOUT TIA

 Article numbers

Designation

Version 
 6AU1810-1BA52-1XA0 SCOUT V5.2 SP1 
 Single license, DVD
V5.2 SP1
 6AU1810-1BA52-1XE0 SCOUT V5.2 SP1 
Upgrade license, DVD
 V5.2 SP1
 6AU1810-1BA52-1XT7 SCOUT V5.2 SP1
 Test license, DVD
 V5.2 SP1
   
 6AU1810-1CA52-1XA0 SCOUT V5.2 SP1 Stand-alone
 Single license, DVD
 V5.2 SP1
 6AU1810-1CA52-1XE0 SCOUT V5.2 SP1 Stand-alone
 Upgrade license, DVD
 V5.2 SP1
 6AU1810-1CA52-1XT7 SCOUT V5.2 SP1 Stand-alone
 Test license, DVD
 V5.2 SP1
   
 6AU1810-1BA52-1XH5

SCOUT V5.2 SP1 (OSD) Online Software Delivery
(E-mail address required for delivery)
Single license, key to download

 V5.2 SP1
 

 6AU1810-1BA52-1XK5

 

SCOUT V5.2 SP1 (OSD) Online Software Delivery
(E-mail address required for delivery)
Upgrade license, key to download

 V5.2 SP1
   
 

 6AU1810-1CA52-1XH5

 

SCOUT V5.2 SP1 stand-alone (OSD) Online Software Delivery
(E-mail address required for delivery)
Single license, key to download

 V5.2 SP1
 

 6AU1810-1CA52-1XK5

SCOUT V5.2 SP1 stand-alone (OSD) Online Software Delivery
(E-mail address required for delivery)
Upgrade license, key to download

 V5.2 SP1

A new license key is required for SCOUT V5.2 SP1.
A license for SCOUT V5.2 may also be used for SCOUT versions V5.1, V4.5, V4.4, V4.3, V4.2, V4.1 and V4.0.


SIMOTION DCC

 Article numbers

Designation

Version 

6AU1810-1JA32-1XA0

SIMOTION DCC full license

 V3.2.1.0 1)
6AU1810-1JA32-1XE0

SIMOTION DCC upgrade license

 V3.2.1.0 1)

1) Note: See also section SIMOTION DCC.


SIMOTION CAMTOOL

 Article numbers

Designation

Version 

6AU1810-0FA41-0XH5

SIMOTION CamTool V4.1 (OSD) Online Software Delivery
(E-mail address required for delivery)
Single license, key to download

V4.2 SP1
(see note)

6AU1810-0FA41-0XK5

SIMOTION CamTool V4.1 (OSD) Online Software Delivery
(E-mail address required for delivery)
Upgrade license, key to download

V4.2 SP1
(see note)

Note
CamTool V4.2 SP1 is only supplied via SCOUT/SCOUT stand-alone and can be installed through the respective setup. CamTool V4.2 SP1 continues to use license key V4.1.
A license for CamTool V4.1 may also be used for versions V3.0 and V2.2.


SIMOTION D

 Article numbers

Designation

Version 

6AU1400-1PA23-0AA0

CompactFlash card (CF) 1 GB for SIMOTION D410-2

with SIMOTION kernel/firmware and SINAMICS S120 drive software; current software release; can be pre-licensed using Z options

 V5.2 SP1

6AU1400-2PA23-0AA0

CompactFlash card (CF) 1 GB for SIMOTION D4x5-2

with SIMOTION kernel/firmware and SINAMICS S120 drive software; current software version; can be pre-licensed using Z options

 V5.2 SP1
 6AU1820-2AG20-0AB0

Runtime License "SINAMICS Safety Integrated Advanced Functions for SIMOTION D"  

Can also be ordered pre-licensed on a SIMOTION D CompactFlash card:
Z option Lxx (xx = Number of licenses)

 ---


SIMOTION C

 Article numbers

Designation

Version 

6AU1720-1KA00-0AA0

MMC 64MB for SIMOTION C240 / C240 PN with SIMOTION kernel/firmware;
can be pre-licensed using Z options

 V5.2 SP1


SIMOTION P320-4 (available in June 2018)    

 Article numbers

Designation

Version 

6AU1320-4DE65-3AF0

SIMOTION P320-4 E
Windows embedded Standard 7 operating system with SIMOTION runtime/kernel installed on internal CFast card.
Delivery with Certificate of License (CoL) for Z options ordered additionally.

 V5.2 SP1

6AU1320-4DS66-3AG0

SIMOTION P320-4 S

Windows 7 Ultimate operating system with SIMOTION runtime/kernel installed on internal solid-state drive (SSD).
Delivery with Certificate of License (CoL) for Z options ordered additionally.

 V5.2 SP1



6. Detailed information on SIMOTION engineering and kernel/firmware/licenses

SIMOTION SCOUT and SCOUT TIA

The scope of delivery of SCOUT version V5.2 SP1 allows SCOUT to be installed in the classic STEP 7 V5.6 environment, as well as SCOUT TIA in the TIA Portal V15.
SCOUT or SCOUT stand-alone and SCOUT TIA V5.2 SP1 can be installed "side-by-side" on a PC.
Only one SCOUT V5.2 license is required.

SIMOTION SCOUT version V5.2 SP1 requires version STEP 7 V5.6 as option package for STEP 7.
SCOUT stand-alone V5.2 SP1 includes STEP 7 components of version V5.6.
SCOUT and SCOUT stand-alone have been released for the operating systems Windows 7 SP1 Professional, Enterprise and Ultimate (64-bit), Windows 10 Pro / Enterprise (64-bit).

SIMOTION SCOUT software releases can be ordered using the article numbers mentioned above. New part orders for older versions are not automatically substituted by SIMOTION version V5.2 SP1.

SIMOTION SCOUT TIA version V5.2 SP1 requires an installation of Totally Integrated Automation Portal V15. SCOUT TIA has been released for the operating systems Windows 7 SP1 Professional, Enterprise and Ultimate (64-bit) as well as Windows 10 Pro / Enterprise (64-bit).

You can find an overview of the versions and significant functional differences regarding "SIMOTION inside the TIA Portal" (SCOUT TIA) here:

  SIMOTION_inside_the_TIA_Portal_-_Details.pdf (443,3 KB)


SIMOTION SCOUT Service Contracts

Users with a valid software update service contract for SCOUT or SCOUT Stand-alone are automatically supplied with SCOUT or SCOUT stand-alone V5.2 SP1 incl. SCOUT TIA after release of the DVDs. Urgently required software can be downloaded via OSD or in SIOS (trial license).
Users without update service can source the current software release with the article numbers listed above.

For more detailed information, please contact your local Siemens representative.


SIMOTION DCC

For use, the appropriate SIMOTION DCC product should be ordered. The SIMOTION DCC product only includes the license for SIMOTION DCC and SINAMICS DCC. Licenses for V2.1, V2.2 SP1, V2.3 and V2.4 remain valid for V3.2 SP1 and can continue to be ordered. Licenses for V2.0 require an upgrade license. DCC for SIMOTION and SINAMICS can be installed using the setup for SCOUT V5.2 SP1 (DCC libraries (DCB) are also automatically installed and the installation of the DCC editor (CFC V9.0) should be activated in the setup).


SIMOTION CamTool V4.2 SP1

The CamTool software is used to generate cams in a user-friendly fashion. CamTool is an option package for SIMOTION SCOUT and is included in the SCOUT software package. CamTool cannot be ordered separately.

With SCOUT TIA, CamTool can also be installed within the scope of the SCOUT TIA installation (optional).

The CamTool should be separately licensed in both cases.


SIMOTION C and SIMOTION D4xx-2

MMC for SIMOTION C and the CF cards for SIMOTION D4xx-2 are supplied with kernel/firmware V5.2 SP1.
Kernel/firmware V5.2 SP1 is available for download in SIOS.


Advanced Safety with SIMOTION D / CX32-2

As of SIMOTION D firmware V5.2 SP1 (SINAMICS Integrated as of V5.1), the "SINAMICS Safety Integrated Advanced Functions for SIMOTION D" license is required for SLP, SP and SCA.
One license per safety axis with Safety Integrated Advanced Functions is required. The license can be used for drives for SIMOTION D and CX32-2 controller extensions. A separate SINAMICS license is available for SINAMICS S120 CU320-2/CU310-2 (see 109753108). 
The Safety Integrated Advanced Functions also include the Safety Integrated Extended Functions.
Licenses for Safety Integrated Advanced Functions are not included in the MultiAxes and Safety Extended Packages and can only be ordered as individual licenses. 


SIMOTION P320-4

The software for the P320-4 with kernel/firmware V5.2 SP1 will be available in June 2018. Storage in SIOS is not permitted for licensing reasons. Please contact your sales department, if needed.
As soon as delivery of P320-4 with V5.2 SP1 takes place, we will inform you again in SIOS.


Firmware Support Package

The device update tool can be used for upgrading SIMOTION C and D from SIMOTION software version V4.1 SP2 to SIMOTION software version V5.2 SP1. Firmware Support Package V5.2 SP1 is required for this.


7. Downloads

The following downloads are available on the Internet Product Support pages:
 
SIMOTION SCOUT, SCOUT stand-alone and SCOUT TIA V5.2 SP1 complete setup, see 109755392
SIMOTION C kernel/firmware V5.2 SP1, see 31263919
SIMOTION D kernel/firmware V5.2 SP1, see 31045047
SIMOTION Firmware Support Package (FWSP) for device update tool, see 33119786


8. Additional information

Please refer to the readme file for additional information about SIMOTION software version V5.2 SP1.

  Liesmich.pdf (514,3 KB)

  Readme.pdf (493,3 KB)

    
SIMOTION at a glance

For frequently asked questions from our range of information, we have created an overview page for you with the most important information about SIMOTION that can be reached with just one click.
Whether you are a new or experienced SIMOTION user – here you will find the most important downloads, manuals, tutorials, FAQs, application examples, etc.

Notes relatives à la sécurité
La protection des installations, systèmes, machines et réseaux contre les cyber-menaces nécessite la réalisation (et le maintien continu) d'un concept global de sécurité IT à la pointe de la technique. Les produits et solutions Siemens ne constituent qu'un élément d'un tel concept. Pour plus d’informations sur la cyber-sécurité, rendez-vous sur
https://www.siemens.com/cybersecurity#Ouraspiration.
Aide pour la statistique
Cette fonction permet de délivrer les identifiants des résultats de la recherche selon la quantité souhaitée (format .txt).

Générer une liste
Copier l'URL
Afficher cette page dans le nouveau design
Poste de commande mySupport
Pages thématiques concernant cette contribution