×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 109755705, Entry date: 04/05/2018
(1)
Rate

Industrial Identification with SIMATIC MV320 and MV340 via RF170C

  • Entry
  • Associated product(s)
The optical handheld readers SIMATIC MV320 and MV340 for 1D and 2D codes enable you to transfer the reading results directly to a SIMATIC PLC. For this purpose, the SIMATIC RF170C communication module can be used. Connection can be established via PROFINET or PROFIBUS.

Besides their function as USB input devices, the optical handheld readers SIMATIC MV320 and MV340 can also be operated using a SIMATIC PLC. Das RFID interface module SIMATIC RF170C (via ET 200pro) allows direct communication between the PLC and the optical handheld reader. The "SIMATIC Ident" standard blocks of the TIA Portal are intended for controlling the functions.

This application example explains how to configure the required modules and provides a function block that demonstrates how to use the SIMATIC Ident blocks for operating the handheld readers MV320 and MV340. You can use the function block directly or adapt it to further requirements.


 

Documentation and sample projects
  Documentation (1,3 MB)
 Registrierung notwendig  Project for STEP 7 V14 SP1 (1,3 MB)

Additional Keywords
serial connection, serial communication, hand scanner

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.