×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 109755814, Entry date: 03/01/2019
(0)
Rate

Update of the licenses and document packages for SIMATIC IPC227E, IPC277E, IPC427D and IPC477D Bundles

  • Entry
  • Associated product(s)
The document packages of the Embedded Bundles with SIMATIC WinCC Runtime Advanced (TIA Portal) and Windows Embedded Standard 7 for SIMATIC IPC227E/IPC277E und SIMATIC IPC427D/IPC477D Panel PC have been updated. The SIMATIC WinCC RT Advanced installation DVD and the license keys have been updated.

Scope of the new license and document package
 
By changing the document packages, it is now possible to update the supplied bundles to the latest version of the SIMATIC software WinCC RT Advanced V15.

The following changes have been performed:

  • Regarding IPC227E and IPC277E, the contents  of the installation DVD for the SIMATIC WinCC Runtime Advanced V15 have been stored on the attached USB Flash Drive.
  • Regarding IPC427D and IPC477D, the installation DVD for the SIMATIC WinCC Runtime Advanced V13 has been replaced by the current version V15.
    The installation DVD and the license key of SIMATIC NET V14 are still attached as usual.
  • The license keys for SIMATIC WinCC Runtime Advanced are now included in version V15.

 
The changes are applied to all new orders placed starting on 19 February 2018.
We do not plan to update the preinstalled software packages.

Hardware

Pre-installed software

New license keys

IPC227E / IPC277E

  • Windows Embedded Standard 7 SP1 (WES7 SP1)
  • WinCC RT Advanced V14
  • Software controller CPU1507S

WinCC RT Advanced V15 (including Recipes and Logging)

 

IPC427D / IPC477D

  • Windows Embedded Standard 7 SP1 (WES7 SP1)
  • WinCC RT Advanced V13 SP1
  • WinAC RTX (F) 2010 SP2
  • SIMATIC Net V12.2

 

WinCC RT Advanced V15 (including Recipes and Logging)

 

Please note - Information regarding the minimum requirements: 


  • Mass storage: SSD or CFAST >= 16 GB
  • RAM: At least 4 GB, Controller Bundle or HMI/Controller Bundle with NVRAM only


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.