×
Siemens Industry Online Support
Siemens AG
文档类型 应用与工具 文档编号 109755892, 文档发布日期 2019年2月27日
(20)
评估

SIMATIC S7-1500T Kinematics Manual Control

  • 文档
  • 涉及产品
The library LKinMCtrl provides manual control functionalities for TO Kinematics with a predefined faceplate for an HMI. This reduces HMI engineering time as all mayor kinematics functions are encapsulated in a single HMI faceplate.

The library LKinMCtrl enabels to perform manual control functionalities and configuration on kinematics technology object via an HMI faceplate without using the engineering system. The faceplate offers a consistent and user-friendly operating concept and can be seamlessly integrated into an existing HMI, as its size is freely adjustable and the general HMI design/style can be applied to the faceplate.

Following benefits are provided with this library:

  • Jog kinematics with different modes
  • Jog / home single axes
  • Clearly displayed error of the kinematics and axes on HMI
  • Monitoring and configuration of zones
  • Configuration of kinematics dynamics and frames
  • Configuration of axis dynamics and position limits
  • Teach kinematics positions in a point table

The faceplate can run on multiple HMIs on the machine as an integrated interlock manages the access to the kinematics. A life-sign is being monitored and deactivates the Manual Control on HMI in case the connection is interrupted. Single functionalities can be activated or deactivated depending on the machine state or the user's authorization level. The faceplate is applicable on all SIMATIC Comfort Panels and Mobile Panels.

Adapt the faceplate to your HMI style


Related Applications

To use the faceplate the following libraries are required:
SIMATIC Axis Control           109749348 
SIMATIC S7-1500T LKinCtrl 109755891  

Further Information
Handling with SIMATIC 109757198 

Additional Keywords
motioncontrol_apc_applications, handling, TO_Kinematics, kinematics technology object, teach


安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.